<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 QUECTEL EC25E LTE module testing on imx6.</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/QUECTEL-EC25E-LTE-module-testing-on-imx6/m-p/720648#M112061</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am testing quectel EC25E LTE module on my imx6 board.quectel LTE module will detect as USB.For this,I need to edit option.c file in kernel.I want to add some hex value of EC25E module and add it in kernel.Then it will detect as usb and i will go ahead on another step.Now problem is there is no file like option.c in my kernel .I have few question about this imx6 kernel.I am using linux 3.0.55 kernel on my board.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1)May I download same kernel version and modify the option.c file and add it in kernel.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;2)If i will add kernel file like this,in future it will affect reset of the functions of the imx6 or not&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So,how to edit option.c and add it in kernel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 01 Mar 2018 11:19:59 GMT</pubDate>
    <dc:creator>selvamurugantha</dc:creator>
    <dc:date>2018-03-01T11:19:59Z</dc:date>
    <item>
      <title>QUECTEL EC25E LTE module testing on imx6.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/QUECTEL-EC25E-LTE-module-testing-on-imx6/m-p/720648#M112061</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am testing quectel EC25E LTE module on my imx6 board.quectel LTE module will detect as USB.For this,I need to edit option.c file in kernel.I want to add some hex value of EC25E module and add it in kernel.Then it will detect as usb and i will go ahead on another step.Now problem is there is no file like option.c in my kernel .I have few question about this imx6 kernel.I am using linux 3.0.55 kernel on my board.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1)May I download same kernel version and modify the option.c file and add it in kernel.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;2)If i will add kernel file like this,in future it will affect reset of the functions of the imx6 or not&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So,how to edit option.c and add it in kernel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 01 Mar 2018 11:19:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/QUECTEL-EC25E-LTE-module-testing-on-imx6/m-p/720648#M112061</guid>
      <dc:creator>selvamurugantha</dc:creator>
      <dc:date>2018-03-01T11:19:59Z</dc:date>
    </item>
  </channel>
</rss>