<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: IMX6UL ADC differential Inputs</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/IMX6UL-ADC-differential-Inputs/m-p/720596#M112057</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi SHAMMI,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In case of the i.MX6UL processor, it has up to two 12-bit ADC modules with up to 10 input channels in total. However, all the channels are single ended; it doesn’t include differential inputs.&lt;/P&gt;&lt;P&gt;You could find a test procedure in the ADC Driver chapter of i.MX Linux Manual document.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Hope this will be useful for you.&lt;BR /&gt;Best regards!&lt;BR /&gt;/Carlos&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 26 Oct 2017 00:46:56 GMT</pubDate>
    <dc:creator>CarlosCasillas</dc:creator>
    <dc:date>2017-10-26T00:46:56Z</dc:date>
    <item>
      <title>IMX6UL ADC differential Inputs</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6UL-ADC-differential-Inputs/m-p/720595#M112056</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Does imx6ul internal ADC has differential inputs ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks &amp;amp; Regards,&lt;/P&gt;&lt;P&gt;SHAMMI&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 25 Oct 2017 11:11:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6UL-ADC-differential-Inputs/m-p/720595#M112056</guid>
      <dc:creator>shammi112</dc:creator>
      <dc:date>2017-10-25T11:11:25Z</dc:date>
    </item>
    <item>
      <title>Re: IMX6UL ADC differential Inputs</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6UL-ADC-differential-Inputs/m-p/720596#M112057</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi SHAMMI,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In case of the i.MX6UL processor, it has up to two 12-bit ADC modules with up to 10 input channels in total. However, all the channels are single ended; it doesn’t include differential inputs.&lt;/P&gt;&lt;P&gt;You could find a test procedure in the ADC Driver chapter of i.MX Linux Manual document.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Hope this will be useful for you.&lt;BR /&gt;Best regards!&lt;BR /&gt;/Carlos&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 26 Oct 2017 00:46:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6UL-ADC-differential-Inputs/m-p/720596#M112057</guid>
      <dc:creator>CarlosCasillas</dc:creator>
      <dc:date>2017-10-26T00:46:56Z</dc:date>
    </item>
  </channel>
</rss>