<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックImx6 Dual Lite Reset Issue</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Imx6-Dual-Lite-Reset-Issue/m-p/720497#M112026</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I use imx6 dual lite board with Green hills integrity OS 11.0.4 and have problem in reset :&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1-When u-boot loads kernel and write reboot command , the system reset and u-boot detect reset issue is watchdog &lt;BR /&gt; but the kernel loaded but the system halted after 16 seconds.&lt;BR /&gt;2-When u-boot loads kernel and push reset button , the system reset and u-boot detect reset issue is POWER &lt;BR /&gt; but the kernel loaded but the system halted after 16 seconds.&lt;BR /&gt;3-When you stop u-boot and write reset command of u-boot ,the u-boot reset and u-boot detect reset issue is watchdog&lt;BR /&gt; and the system continue correctly and loads kernel and works fine&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 20 Nov 2017 16:59:25 GMT</pubDate>
    <dc:creator>karimbakir</dc:creator>
    <dc:date>2017-11-20T16:59:25Z</dc:date>
    <item>
      <title>Imx6 Dual Lite Reset Issue</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Imx6-Dual-Lite-Reset-Issue/m-p/720497#M112026</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I use imx6 dual lite board with Green hills integrity OS 11.0.4 and have problem in reset :&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1-When u-boot loads kernel and write reboot command , the system reset and u-boot detect reset issue is watchdog &lt;BR /&gt; but the kernel loaded but the system halted after 16 seconds.&lt;BR /&gt;2-When u-boot loads kernel and push reset button , the system reset and u-boot detect reset issue is POWER &lt;BR /&gt; but the kernel loaded but the system halted after 16 seconds.&lt;BR /&gt;3-When you stop u-boot and write reset command of u-boot ,the u-boot reset and u-boot detect reset issue is watchdog&lt;BR /&gt; and the system continue correctly and loads kernel and works fine&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 20 Nov 2017 16:59:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Imx6-Dual-Lite-Reset-Issue/m-p/720497#M112026</guid>
      <dc:creator>karimbakir</dc:creator>
      <dc:date>2017-11-20T16:59:25Z</dc:date>
    </item>
    <item>
      <title>Re: Imx6 Dual Lite Reset Issue</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Imx6-Dual-Lite-Reset-Issue/m-p/720498#M112027</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi karim&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;for reliable reboot it is necessary to implement reset circuit as it is done&lt;/P&gt;&lt;P&gt;on Sabre SD schematic spf-27392 p.21 (U507), also resetting pmic with PWRON:&lt;/P&gt;&lt;P&gt;Schematics (1)&lt;BR /&gt;i.MX6_SABRE_SDP_DESIGNFILES&lt;BR /&gt;&lt;A class="jive-link-external-small" href="https://community.nxp.com/external-link.jspa?url=http%3A%2F%2Fwww.nxp.com%2Fproducts%2Fsoftware-and-tools%2Fhardware-development-tools%2Fsabre-development-system%2Fsabre-platform-for-smart-devices-based-on-the-i.mx-6-series%3ARDIMX6SABREPLAT%3Ffpsp%3D1%26tab%3DDesign_Tools_Tab" rel="nofollow" target="_blank"&gt;http://www.nxp.com/products/software-and-tools/hardware-development-tools/sabre-development-system/sabre-platform-for-smart-devices-based-on-the-i.mx-6-series:RDIMX6SABREPLAT?fpsp=1&amp;amp;tab=Design_Tools_Tab&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 22 Nov 2017 07:06:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Imx6-Dual-Lite-Reset-Issue/m-p/720498#M112027</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2017-11-22T07:06:20Z</dc:date>
    </item>
  </channel>
</rss>