<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 U-Boot RAM Test</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/U-Boot-RAM-Test/m-p/719538#M111828</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;BR /&gt; &lt;BR /&gt;I have an iMX6UL board,&lt;BR /&gt;i am doing U-Boot Ram Test RAM address range start from 0x80000000 to 0x90000000.&lt;BR /&gt;i need to find out the safe address range to perform U-boot- RAM test,&lt;BR /&gt;because some portion of Ram is containig U-Boot.&lt;BR /&gt;if i will perform RAM test for complete RAM then there are chances of RAM crash&lt;BR /&gt;to avoid this i need address range to for which i can perform test.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Thank you :)&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 13 Dec 2017 08:56:44 GMT</pubDate>
    <dc:creator>anshulkhare</dc:creator>
    <dc:date>2017-12-13T08:56:44Z</dc:date>
    <item>
      <title>U-Boot RAM Test</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/U-Boot-RAM-Test/m-p/719538#M111828</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;BR /&gt; &lt;BR /&gt;I have an iMX6UL board,&lt;BR /&gt;i am doing U-Boot Ram Test RAM address range start from 0x80000000 to 0x90000000.&lt;BR /&gt;i need to find out the safe address range to perform U-boot- RAM test,&lt;BR /&gt;because some portion of Ram is containig U-Boot.&lt;BR /&gt;if i will perform RAM test for complete RAM then there are chances of RAM crash&lt;BR /&gt;to avoid this i need address range to for which i can perform test.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Thank you :)&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 13 Dec 2017 08:56:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/U-Boot-RAM-Test/m-p/719538#M111828</guid>
      <dc:creator>anshulkhare</dc:creator>
      <dc:date>2017-12-13T08:56:44Z</dc:date>
    </item>
    <item>
      <title>Re: U-Boot RAM Test</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/U-Boot-RAM-Test/m-p/719539#M111829</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;in the following file you will find &lt;SPAN style="font-size: 10.0pt; color: black;"&gt;CONFIG_SYS_TEXT_BASE which indicates uboot address.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;lt;build-dir&amp;gt;/tmp/work/&amp;lt;poky-linux-gnueabi&amp;gt;/uboot-imx/&amp;lt;version&amp;gt;/git/include/configs/&amp;lt;board&amp;gt;.h&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Regards,&lt;BR /&gt;Carlos&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 15 Dec 2017 22:03:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/U-Boot-RAM-Test/m-p/719539#M111829</guid>
      <dc:creator>Carlos_Musich</dc:creator>
      <dc:date>2017-12-15T22:03:10Z</dc:date>
    </item>
  </channel>
</rss>