<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Creating .sdcard image manually in host PC  in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Creating-sdcard-image-manually-in-host-PC/m-p/719410#M111805</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi'&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;I have following binaries&lt;/P&gt;&lt;P&gt;• Linux OS kernel image (zImage)&lt;/P&gt;&lt;P&gt;• Device tree file (*.dtb)&lt;/P&gt;&lt;P&gt;• U-Boot bootloader image&lt;/P&gt;&lt;P&gt;• Root file system (*.ext3 or *.ext4)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;How I can create an &lt;STRONG&gt;.sdcard&lt;/STRONG&gt; image, which contains all these four images properly configured for an SD card by manually in my &lt;STRONG&gt;Ubuntu&lt;/STRONG&gt; PC? What command I can use? If you have any script it is more helpful.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When I searched this question, I got the link &lt;A href="https://community.nxp.com/docs/DOC-105521"&gt;Guide to the .sdcard format&lt;/A&gt; . But he explained configuration in yocto to build .sdcard image.&lt;/P&gt;&lt;P&gt;In yocto build I found IMAGE_FSTYPES="tar.bz2 ext3 sdcard" in some .conf file. But I didn't get where is the script to generate .sdcard image.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I want to do .sdcard image manually in my Ubuntu PC with the commands .&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks and Regards&lt;/P&gt;&lt;P&gt;Devendra&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 02 May 2018 11:06:45 GMT</pubDate>
    <dc:creator>devendradevadig</dc:creator>
    <dc:date>2018-05-02T11:06:45Z</dc:date>
    <item>
      <title>Creating .sdcard image manually in host PC</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Creating-sdcard-image-manually-in-host-PC/m-p/719410#M111805</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi'&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;I have following binaries&lt;/P&gt;&lt;P&gt;• Linux OS kernel image (zImage)&lt;/P&gt;&lt;P&gt;• Device tree file (*.dtb)&lt;/P&gt;&lt;P&gt;• U-Boot bootloader image&lt;/P&gt;&lt;P&gt;• Root file system (*.ext3 or *.ext4)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;How I can create an &lt;STRONG&gt;.sdcard&lt;/STRONG&gt; image, which contains all these four images properly configured for an SD card by manually in my &lt;STRONG&gt;Ubuntu&lt;/STRONG&gt; PC? What command I can use? If you have any script it is more helpful.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When I searched this question, I got the link &lt;A href="https://community.nxp.com/docs/DOC-105521"&gt;Guide to the .sdcard format&lt;/A&gt; . But he explained configuration in yocto to build .sdcard image.&lt;/P&gt;&lt;P&gt;In yocto build I found IMAGE_FSTYPES="tar.bz2 ext3 sdcard" in some .conf file. But I didn't get where is the script to generate .sdcard image.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I want to do .sdcard image manually in my Ubuntu PC with the commands .&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks and Regards&lt;/P&gt;&lt;P&gt;Devendra&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 02 May 2018 11:06:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Creating-sdcard-image-manually-in-host-PC/m-p/719410#M111805</guid>
      <dc:creator>devendradevadig</dc:creator>
      <dc:date>2018-05-02T11:06:45Z</dc:date>
    </item>
    <item>
      <title>Re: Creating .sdcard image manually in host PC</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Creating-sdcard-image-manually-in-host-PC/m-p/719411#M111806</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Devendra,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You would need to go to the recipes in Yocto that have the parameters to create the .sdcard image.&lt;/P&gt;&lt;P&gt;You can see the code that creates the .sdcard file on&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;lt;BSP_DIR&amp;gt;/&amp;lt;BUILD_DIR&amp;gt;/sources/meta-fsl-arm/classes/image_types_fsl.bbclass&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You could start from there at least in overall steps needed to get the file created.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope this helps!&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 02 May 2018 16:33:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Creating-sdcard-image-manually-in-host-PC/m-p/719411#M111806</guid>
      <dc:creator>gusarambula</dc:creator>
      <dc:date>2018-05-02T16:33:10Z</dc:date>
    </item>
    <item>
      <title>Re: Creating .sdcard image manually in host PC</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Creating-sdcard-image-manually-in-host-PC/m-p/719412#M111807</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;AndroidSDCARDMirrorCreator&lt;/P&gt;&lt;P&gt;&lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-329596"&gt;https://community.nxp.com/docs/DOC-329596&lt;/A&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 03 May 2018 02:49:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Creating-sdcard-image-manually-in-host-PC/m-p/719412#M111807</guid>
      <dc:creator>BiyongSUN</dc:creator>
      <dc:date>2018-05-03T02:49:25Z</dc:date>
    </item>
  </channel>
</rss>