<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックIMX7D USB_OTG_VBUS allowed enable power level?</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/IMX7D-USB-OTG-VBUS-allowed-enable-power-level/m-p/719104#M111766</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Support,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We are checking the property of this pin and we might need to use 3.3V instead of 5V from USB connector. What's the limitation? Is 3.3V of for it?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 14 Dec 2017 03:29:13 GMT</pubDate>
    <dc:creator>frankyhsu</dc:creator>
    <dc:date>2017-12-14T03:29:13Z</dc:date>
    <item>
      <title>IMX7D USB_OTG_VBUS allowed enable power level?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX7D-USB-OTG-VBUS-allowed-enable-power-level/m-p/719104#M111766</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Support,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We are checking the property of this pin and we might need to use 3.3V instead of 5V from USB connector. What's the limitation? Is 3.3V of for it?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 14 Dec 2017 03:29:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX7D-USB-OTG-VBUS-allowed-enable-power-level/m-p/719104#M111766</guid>
      <dc:creator>frankyhsu</dc:creator>
      <dc:date>2017-12-14T03:29:13Z</dc:date>
    </item>
    <item>
      <title>Re: IMX7D USB_OTG_VBUS allowed enable power level?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX7D-USB-OTG-VBUS-allowed-enable-power-level/m-p/719105#M111767</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&amp;nbsp; In order to meet specs, minimum VBUS is 4.75 V; maximum is 5.25V. &lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&amp;nbsp;Generally, i.MX7 can work in device mode without VBUS, but it is needed to modify &lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;software to disable VBUS detection.&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&amp;nbsp;&amp;nbsp; But the following impacts should be taken in consideration:&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&amp;nbsp;1) i.MX7 may NOT detect plug in/out events, because the interrupt is triggered &lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&amp;nbsp; by the VBUS level;&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;2) i.MX7 USB may NOT work at low power mode, because VBUS functions as the &lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&amp;nbsp; wake-up source.&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Yuri&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/message/586582"&gt;https://community.nxp.com/message/586582&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 14 Dec 2017 04:04:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX7D-USB-OTG-VBUS-allowed-enable-power-level/m-p/719105#M111767</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2017-12-14T04:04:02Z</dc:date>
    </item>
    <item>
      <title>Re: IMX7D USB_OTG_VBUS allowed enable power level?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX7D-USB-OTG-VBUS-allowed-enable-power-level/m-p/719106#M111768</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;We see that the 3.3V input and even lower to 1.8V, it can still work &lt;/P&gt;&lt;P&gt;unless we connect nothing. So, NXP can still accept the 4.75 as the &lt;/P&gt;&lt;P&gt;minimum?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Franky Hsu&lt;/P&gt;&lt;P&gt;Sercomm Corp.&lt;/P&gt;&lt;P&gt;2F, No.3-1, YuanQu St., Nankang, Taipei 115, Taiwan&lt;/P&gt;&lt;P&gt;+886-2-26553988 #2552&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;寄件者:         "Yuri" &amp;lt;admin@community.nxp.com&amp;gt;&lt;/P&gt;&lt;P&gt;收件者:         "Franky Hsu" &amp;lt;franky_hsu@sercomm.com&amp;gt;, &lt;/P&gt;&lt;P&gt;日期:   2017/12/14 下午 12:04&lt;/P&gt;&lt;P&gt;主旨:   Re:  - Re: IMX7D USB_OTG_VBUS allowed enable power &lt;/P&gt;&lt;P&gt;level?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;NXP Community &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Re: IMX7D USB_OTG_VBUS allowed enable power level? &lt;/P&gt;&lt;P&gt;reply from Yuri Muhin in i.MX Community - View the full discussion&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt; &lt;/P&gt;&lt;P&gt;  In order to meet specs, minimum VBUS is 4.75 V; maximum is 5.25V. &lt;/P&gt;&lt;P&gt; Generally, i.MX7 can work in device mode without VBUS, but it is needed &lt;/P&gt;&lt;P&gt;to modify &lt;/P&gt;&lt;P&gt;software to disable VBUS detection.&lt;/P&gt;&lt;P&gt;   But the following impacts should be taken in consideration:&lt;/P&gt;&lt;P&gt; 1) i.MX7 may NOT detect plug in/out events, because the interrupt is &lt;/P&gt;&lt;P&gt;triggered &lt;/P&gt;&lt;P&gt;  by the VBUS level;&lt;/P&gt;&lt;P&gt;2) i.MX7 USB may NOT work at low power mode, because VBUS functions as the &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;  wake-up source.&lt;/P&gt;&lt;P&gt; &lt;/P&gt;&lt;P&gt;Have a great day,&lt;/P&gt;&lt;P&gt;Yuri&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 14 Dec 2017 04:14:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX7D-USB-OTG-VBUS-allowed-enable-power-level/m-p/719106#M111768</guid>
      <dc:creator>frankyhsu</dc:creator>
      <dc:date>2017-12-14T04:14:30Z</dc:date>
    </item>
    <item>
      <title>Re: IMX7D USB_OTG_VBUS allowed enable power level?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX7D-USB-OTG-VBUS-allowed-enable-power-level/m-p/719107#M111769</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp;You may use Your configuration - it does not violate (hardware) maximum ratings,&lt;/P&gt;&lt;P&gt;but do not forget about possible (software) impacts.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Yuri.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 14 Dec 2017 09:16:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX7D-USB-OTG-VBUS-allowed-enable-power-level/m-p/719107#M111769</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2017-12-14T09:16:27Z</dc:date>
    </item>
  </channel>
</rss>