<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: adb device serial no issue</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/adb-device-serial-no-issue/m-p/719100#M111765</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Are you using our Sabre-SD board and our Android BSP?&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;This is because I tested the Android image and it has the serial number using the adb tool. I don't have the same problem as you.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Best regards,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Diego.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 12 Jan 2018 18:52:00 GMT</pubDate>
    <dc:creator>diegoadrian</dc:creator>
    <dc:date>2018-01-12T18:52:00Z</dc:date>
    <item>
      <title>adb device serial no issue</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/adb-device-serial-no-issue/m-p/719099#M111764</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;I am using Android-marshmallow on IMX7D.&lt;/P&gt;&lt;P&gt;I got below observations at the time of using adb commands.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;adb devices&lt;/P&gt;&lt;P&gt;???????? &amp;nbsp; &amp;nbsp; device&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am able to login to IMX7D board using "adb shell" .&lt;/P&gt;&lt;P&gt;But why its not showing any serial no.&lt;/P&gt;&lt;P&gt;"serial no" is required instead of " ????".&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any suggestion on this.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks &amp;amp; regards&lt;/P&gt;&lt;P&gt;Surya&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 12 Jan 2018 12:15:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/adb-device-serial-no-issue/m-p/719099#M111764</guid>
      <dc:creator>suryapradhan</dc:creator>
      <dc:date>2018-01-12T12:15:35Z</dc:date>
    </item>
    <item>
      <title>Re: adb device serial no issue</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/adb-device-serial-no-issue/m-p/719100#M111765</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Are you using our Sabre-SD board and our Android BSP?&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;This is because I tested the Android image and it has the serial number using the adb tool. I don't have the same problem as you.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Best regards,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Diego.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 12 Jan 2018 18:52:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/adb-device-serial-no-issue/m-p/719100#M111765</guid>
      <dc:creator>diegoadrian</dc:creator>
      <dc:date>2018-01-12T18:52:00Z</dc:date>
    </item>
  </channel>
</rss>