<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic i.MX7 Dual Maximum UART Baud Rate in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-MX7-Dual-Maximum-UART-Baud-Rate/m-p/718989#M111737</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;What is the maximum baud rate for UARTs on the i.MX7 Dual (for both the A cores and the M core)?&amp;nbsp;&amp;nbsp;We&amp;nbsp;are looking at running at 5Mbps.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The family guide seems to imply that it is based on the "module_clock."&amp;nbsp; Is this UART1_CLK_ROOT, etc listed in Table 5-11?&amp;nbsp; This table seems to imply that the maximum clock root frequency is 80MHz.&amp;nbsp;&amp;nbsp;If the 16x higher clock frequency from 14.3.4.2.2 is required for higher frequencies, this means the maximum baud rate is 5MBps.&amp;nbsp; Is this correct?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;15.3.4.2.2 Maximum Baud Rate&lt;/P&gt;&lt;P&gt;The max baud rate the UART can support is determined by the max frequency of the module_clock. For example, if the SoC can provide the fastest module_clock 66.5 MHz, the UART can transmit and receive serial data with the maximum baud rate 66.5M/16 = 4.15 Mbit/s. The UART supports serial IR interface low speed. In the low speed IrDA mode, the max baud rate is 115.2 Kbit/s. To support the 115.2 Kbit/s, module_clock frequency must be higher or equal to 1.8432 MHz.&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;DIV class=""&gt;&lt;DIV class=""&gt;&lt;TABLE&gt;&lt;TBODY&gt;&lt;TR class=""&gt;&lt;TD class=""&gt;&lt;/TD&gt;&lt;/TR&gt;&lt;/TBODY&gt;&lt;/TABLE&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 24 Oct 2017 20:51:22 GMT</pubDate>
    <dc:creator>adrianamickols</dc:creator>
    <dc:date>2017-10-24T20:51:22Z</dc:date>
    <item>
      <title>i.MX7 Dual Maximum UART Baud Rate</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX7-Dual-Maximum-UART-Baud-Rate/m-p/718989#M111737</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;What is the maximum baud rate for UARTs on the i.MX7 Dual (for both the A cores and the M core)?&amp;nbsp;&amp;nbsp;We&amp;nbsp;are looking at running at 5Mbps.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The family guide seems to imply that it is based on the "module_clock."&amp;nbsp; Is this UART1_CLK_ROOT, etc listed in Table 5-11?&amp;nbsp; This table seems to imply that the maximum clock root frequency is 80MHz.&amp;nbsp;&amp;nbsp;If the 16x higher clock frequency from 14.3.4.2.2 is required for higher frequencies, this means the maximum baud rate is 5MBps.&amp;nbsp; Is this correct?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;15.3.4.2.2 Maximum Baud Rate&lt;/P&gt;&lt;P&gt;The max baud rate the UART can support is determined by the max frequency of the module_clock. For example, if the SoC can provide the fastest module_clock 66.5 MHz, the UART can transmit and receive serial data with the maximum baud rate 66.5M/16 = 4.15 Mbit/s. The UART supports serial IR interface low speed. In the low speed IrDA mode, the max baud rate is 115.2 Kbit/s. To support the 115.2 Kbit/s, module_clock frequency must be higher or equal to 1.8432 MHz.&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;DIV class=""&gt;&lt;DIV class=""&gt;&lt;TABLE&gt;&lt;TBODY&gt;&lt;TR class=""&gt;&lt;TD class=""&gt;&lt;/TD&gt;&lt;/TR&gt;&lt;/TBODY&gt;&lt;/TABLE&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 24 Oct 2017 20:51:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX7-Dual-Maximum-UART-Baud-Rate/m-p/718989#M111737</guid>
      <dc:creator>adrianamickols</dc:creator>
      <dc:date>2017-10-24T20:51:22Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX7 Dual Maximum UART Baud Rate</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX7-Dual-Maximum-UART-Baud-Rate/m-p/718990#M111738</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Adriana&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;this understanding is correct, maximum baud rate is 5MBps and uart is the same&lt;/P&gt;&lt;P&gt;as in i.MX6UL, i.MX6SX processors.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 25 Oct 2017 23:03:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX7-Dual-Maximum-UART-Baud-Rate/m-p/718990#M111738</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2017-10-25T23:03:45Z</dc:date>
    </item>
  </channel>
</rss>