<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Hobbit board IMX6Q MFGTOOL2 Install Ubuntu</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Hobbit-board-IMX6Q-MFGTOOL2-Install-Ubuntu/m-p/718445#M111633</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear All,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have Hobbit board from POSLAB, and I have the mfgtools for this board from the vendor to install ubuntu on hobbit board. I turn the board on with serial downloader mode, then I open mfgtool2.exe. The device is detected, then I click 'Start'. It finish smoothly. I click stop, it's said "Linux File-Stor Gadget USB Device". But when I restart with eMMC boot, it shows nothing. Even not detected on usbtreeview. Any suggestion? The mfgtools.log attached.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Edit:&lt;BR /&gt;Not sure, but now, after restart, it was detected as USB Input Device - HID (even I'm not boot it as Serial Downloader Mode).&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 10 Apr 2018 07:17:02 GMT</pubDate>
    <dc:creator>kovzone</dc:creator>
    <dc:date>2018-04-10T07:17:02Z</dc:date>
    <item>
      <title>Hobbit board IMX6Q MFGTOOL2 Install Ubuntu</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Hobbit-board-IMX6Q-MFGTOOL2-Install-Ubuntu/m-p/718445#M111633</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear All,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have Hobbit board from POSLAB, and I have the mfgtools for this board from the vendor to install ubuntu on hobbit board. I turn the board on with serial downloader mode, then I open mfgtool2.exe. The device is detected, then I click 'Start'. It finish smoothly. I click stop, it's said "Linux File-Stor Gadget USB Device". But when I restart with eMMC boot, it shows nothing. Even not detected on usbtreeview. Any suggestion? The mfgtools.log attached.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Edit:&lt;BR /&gt;Not sure, but now, after restart, it was detected as USB Input Device - HID (even I'm not boot it as Serial Downloader Mode).&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 10 Apr 2018 07:17:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Hobbit-board-IMX6Q-MFGTOOL2-Install-Ubuntu/m-p/718445#M111633</guid>
      <dc:creator>kovzone</dc:creator>
      <dc:date>2018-04-10T07:17:02Z</dc:date>
    </item>
    <item>
      <title>Re: Hobbit board IMX6Q MFGTOOL2 Install Ubuntu</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Hobbit-board-IMX6Q-MFGTOOL2-Install-Ubuntu/m-p/718446#M111634</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;which .vbs do you choose? try to confirm if you use the correct settings for emmc, maybe your tool's default setting is for sd card, pls double&amp;nbsp; check it.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 11 Apr 2018 08:54:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Hobbit-board-IMX6Q-MFGTOOL2-Install-Ubuntu/m-p/718446#M111634</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2018-04-11T08:54:54Z</dc:date>
    </item>
    <item>
      <title>Re: Hobbit board IMX6Q MFGTOOL2 Install Ubuntu</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Hobbit-board-IMX6Q-MFGTOOL2-Install-Ubuntu/m-p/718447#M111635</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;It's not using vbs, it's custom from the POSLAB. It's called "Ubuntu-SabreSD-eMMC" on the LIST. In case you want to know the ucl2.xml, it's attached.&lt;/P&gt;&lt;P&gt;I've tried also using mfgtool2-yocto-mx-sabresd-emmc.vbs from NXP, the oneiric.tgz become the source of the problem. I changed it with trusty.tgz from POSLAB, and it's finished smoothly, but still, after restart, it's nothing. I've tried to install&amp;nbsp;the board with Android using mfgtool, it's working.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 11 Apr 2018 09:29:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Hobbit-board-IMX6Q-MFGTOOL2-Install-Ubuntu/m-p/718447#M111635</guid>
      <dc:creator>kovzone</dc:creator>
      <dc:date>2018-04-11T09:29:53Z</dc:date>
    </item>
    <item>
      <title>Re: Hobbit board IMX6Q MFGTOOL2 Install Ubuntu</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Hobbit-board-IMX6Q-MFGTOOL2-Install-Ubuntu/m-p/718448#M111636</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Our company need to develop this board into Linux (Ubuntu, Arch Linux, or Debian) because we will need thousands of it for our client.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 12 Apr 2018 00:59:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Hobbit-board-IMX6Q-MFGTOOL2-Install-Ubuntu/m-p/718448#M111636</guid>
      <dc:creator>kovzone</dc:creator>
      <dc:date>2018-04-12T00:59:25Z</dc:date>
    </item>
    <item>
      <title>Re: Hobbit board IMX6Q MFGTOOL2 Install Ubuntu</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Hobbit-board-IMX6Q-MFGTOOL2-Install-Ubuntu/m-p/718449#M111637</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I don't have the third party board to test for you, when you program ubuntu image to board by mfgtoo, is it sucessful? any log file for that? &lt;/P&gt;&lt;P&gt;"after restart, it's nothing" do you mean that you couldn't get any uboot information? how about try to use dd command?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 12 Apr 2018 09:42:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Hobbit-board-IMX6Q-MFGTOOL2-Install-Ubuntu/m-p/718449#M111637</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2018-04-12T09:42:03Z</dc:date>
    </item>
    <item>
      <title>Re: Hobbit board IMX6Q MFGTOOL2 Install Ubuntu</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Hobbit-board-IMX6Q-MFGTOOL2-Install-Ubuntu/m-p/718450#M111638</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Have you check the mfgtool.log at the first post? Yes, it's successful. What kind of log do you mean? I don't know, it's just nothing detected from the board. USB didn't detect any device. How could I get the uboot information? From terminal like Hyperterminal or Tera Term?&amp;nbsp;I'm still working on enabling the uart communication, because the board only have USB-OTG port. No USB-to-UART. I'll purchase RS232 to USB, i hope it'll works.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Here's the Mfgtools I used if you want to check it.&amp;nbsp;&lt;BR /&gt;&lt;A class="link-titled" href="https://1drv.ms/u/s!AjioG0i8juj_wdQ4jlGmdRwekdgODg" title="https://1drv.ms/u/s!AjioG0i8juj_wdQ4jlGmdRwekdgODg"&gt;Microsoft OneDrive - Access files anywhere. Create docs with free Office Online.&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 12 Apr 2018 10:05:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Hobbit-board-IMX6Q-MFGTOOL2-Install-Ubuntu/m-p/718450#M111638</guid>
      <dc:creator>kovzone</dc:creator>
      <dc:date>2018-04-12T10:05:37Z</dc:date>
    </item>
  </channel>
</rss>