<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Enabling Power on Self Test (POST) IMx6solox in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Enabling-Power-on-Self-Test-POST-IMx6solox/m-p/717919#M111577</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks for the response Igor,&lt;/P&gt;&lt;P&gt;we are looking for some thing like POST to do bare minimal test on power up.&lt;/P&gt;&lt;P&gt;if POST is not supported do we have any other option for self test.&lt;/P&gt;&lt;P&gt;For 1 Gbyte DDR ram test i see there is a mtest, but which is very slow.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;thanks&lt;/P&gt;&lt;P&gt;Niranjan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 25 Oct 2017 12:08:52 GMT</pubDate>
    <dc:creator>niranjanbc</dc:creator>
    <dc:date>2017-10-25T12:08:52Z</dc:date>
    <item>
      <title>Enabling Power on Self Test (POST) IMx6solox</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Enabling-Power-on-Self-Test-POST-IMx6solox/m-p/717917#M111575</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;I am looking to enable the "POST" (POST_CONFIG) in U-boot running on IMX6SoloX, to enable that i need non volatile memory address for _POST_WORD_ADDR. do we have any solution for that. can use the NOR flash address i have my board or it should be onchip memory only.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;THANKS&lt;/P&gt;&lt;P&gt;Niranjan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 24 Oct 2017 15:09:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Enabling-Power-on-Self-Test-POST-IMx6solox/m-p/717917#M111575</guid>
      <dc:creator>niranjanbc</dc:creator>
      <dc:date>2017-10-24T15:09:05Z</dc:date>
    </item>
    <item>
      <title>Re: Enabling Power on Self Test (POST) IMx6solox</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Enabling-Power-on-Self-Test-POST-IMx6solox/m-p/717918#M111576</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Niranjan&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am afraid "POST" is not supported in nxp uboot releases and&lt;BR /&gt;this may be posted on uboot mail list&lt;BR /&gt;&lt;A class="jive-link-external-small" href="https://community.nxp.com/external-link.jspa?url=https%3A%2F%2Flists.denx.de%2Flistinfo%2Fu-boot" rel="nofollow" target="_blank"&gt;https://lists.denx.de/listinfo/u-boot&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 25 Oct 2017 01:12:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Enabling-Power-on-Self-Test-POST-IMx6solox/m-p/717918#M111576</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2017-10-25T01:12:22Z</dc:date>
    </item>
    <item>
      <title>Re: Enabling Power on Self Test (POST) IMx6solox</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Enabling-Power-on-Self-Test-POST-IMx6solox/m-p/717919#M111577</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks for the response Igor,&lt;/P&gt;&lt;P&gt;we are looking for some thing like POST to do bare minimal test on power up.&lt;/P&gt;&lt;P&gt;if POST is not supported do we have any other option for self test.&lt;/P&gt;&lt;P&gt;For 1 Gbyte DDR ram test i see there is a mtest, but which is very slow.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;thanks&lt;/P&gt;&lt;P&gt;Niranjan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 25 Oct 2017 12:08:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Enabling-Power-on-Self-Test-POST-IMx6solox/m-p/717919#M111577</guid>
      <dc:creator>niranjanbc</dc:creator>
      <dc:date>2017-10-25T12:08:52Z</dc:date>
    </item>
  </channel>
</rss>