<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: Pin Config vs Pin Mux</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Pin-Config-vs-Pin-Mux/m-p/717580#M111524</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Lars&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;daisy functionality is described in 8.2.3.3 Daisy chain - multi pads driving same&lt;/P&gt;&lt;P&gt;module input pin i.MX7D Reference Manual &lt;/P&gt;&lt;P&gt;&lt;A class="jive-link-external-small" href="https://community.nxp.com/external-link.jspa?url=http%3A%2F%2Fcache.nxp.com%2Ffiles%2F32bit%2Fdoc%2Fref_manual%2FIMX7DRM.pdf" rel="nofollow" target="_blank"&gt;http://cache.nxp.com/files/32bit/doc/ref_manual/IMX7DRM.pdf&lt;/A&gt;&lt;BR /&gt;and used for some modules like uart. It is not used for i2c so seems its settings&lt;/P&gt;&lt;P&gt;can be changed.&lt;/P&gt;&lt;P&gt;**PAD_CTL_PAD iomux settings greatly depends on customer layout and usage,&lt;/P&gt;&lt;P&gt;so these settings should be adjusted by customer himself. As starting point one&lt;/P&gt;&lt;P&gt;can use default settings.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 06 Feb 2018 05:12:12 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2018-02-06T05:12:12Z</dc:date>
    <item>
      <title>Pin Config vs Pin Mux</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Pin-Config-vs-Pin-Mux/m-p/717579#M111523</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello community,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;the RTOS BSP comes with a lot of example code. Even examples without freeRTOS are included.&lt;/P&gt;&lt;P&gt;This is really helpful, thumbs up!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Most examples call a "hardware_init()" function that is usually located in an additional hardware_init.c file.&lt;BR /&gt;This function sets up clocks and peripherals. I have a question on the peripheral pin mux setup:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;From an I2C example in the BSP:&lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;void configure_i2c_pins(I2C_Type* base){&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;switch((uint32_t)base)&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;{&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;case I2C1_BASE:&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;// I2C1 iomux configuration&lt;BR /&gt;&lt;SPAN style="background-color: #f6f6f6;"&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;IOMUXC_SW_MUX_CTL_PAD_I2C2_SCL = &lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;IOMUXC_SW_MUX_CTL_PAD_I2C2_SCL_MUX_MODE(0) |&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;IOMUXC_SW_MUX_CTL_PAD_I2C2_SCL_SION_MASK;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;IOMUXC_SW_MUX_CTL_PAD_I2C2_SDA = &lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;IOMUXC_SW_MUX_CTL_PAD_I2C2_SDA_MUX_MODE(0) |&lt;BR /&gt; &amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;IOMUXC_SW_MUX_CTL_PAD_I2C2_SDA_SION_MASK;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;IOMUXC_I2C2_SCL_SELECT_INPUT = IOMUXC_I2C2_SCL_SELECT_INPUT_DAISY(1);&lt;BR /&gt; &amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;IOMUXC_I2C2_SDA_SELECT_INPUT = IOMUXC_I2C2_SDA_SELECT_INPUT_DAISY(1);&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;IOMUXC_SW_PAD_CTL_PAD_I2C2_SCL = IOMUXC_SW_PAD_CTL_PAD_I2C2_SCL_PE_MASK |&lt;BR /&gt; &amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;IOMUXC_SW_PAD_CTL_PAD_I2C2_SCL_PS(3) |&lt;BR /&gt; &amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;IOMUXC_SW_PAD_CTL_PAD_I2C2_SCL_DSE(0) |&lt;BR /&gt; &amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;IOMUXC_SW_PAD_CTL_PAD_I2C2_SCL_HYS_MASK;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp;IOMUXC_SW_PAD_CTL_PAD_I2C2_SDA = &lt;BR /&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp;IOMUXC_SW_PAD_CTL_PAD_I2C2_SDA_PE_MASK |&lt;BR /&gt; &amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;IOMUXC_SW_PAD_CTL_PAD_I2C2_SDA_PS(3) |&lt;BR /&gt; &amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;IOMUXC_SW_PAD_CTL_PAD_I2C2_SDA_DSE(0) |&lt;BR /&gt; &amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;IOMUXC_SW_PAD_CTL_PAD_I2C2_SDA_HYS_MASK;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;break;&lt;/P&gt;&lt;P&gt;[...]&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The Pins tool output looks very different from the example above:&lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;/* Input Select (DAISY) Field: Selecting Pad: UART2_RX_DATA Mode: ALT1 for I2C2_SCL */&lt;BR /&gt;HW_IOMUXC_I2C2_SCL_SELECT_INPUT_WR(&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;IOMUXC_BASE,&lt;BR /&gt; &amp;nbsp;&amp;nbsp;&amp;nbsp;BF_IOMUXC_I2C2_SCL_SELECT_INPUT_DAISY(&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;BV_IOMUXC_I2C2_SCL_SELECT_INPUT_DAISY_UART2_RX_DATA_ALT1));&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;/* Input Select (DAISY) Field: Selecting Pad: UART2_TX_DATA Mode: ALT1 for I2C2_SDA */&lt;BR /&gt; HW_IOMUXC_I2C2_SDA_SELECT_INPUT_WR(&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;IOMUXC_BASE,&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;BF_IOMUXC_I2C2_SDA_SELECT_INPUT_DAISY(&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;BV_IOMUXC_I2C2_SDA_SELECT_INPUT_DAISY_UART2_TX_DATA_ALT1));&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So it seems like the file generated by Pins is only setting up the SELECT_INPUT parts.&lt;/P&gt;&lt;P&gt;What happens with the additional settings (containing ...PAD_CTL_PAD...)?&lt;/P&gt;&lt;P&gt;May I simply replace&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="background-color: #f6f6f6;"&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;IOMUXC_I2C2_SCL_SELECT_INPUT = IOMUXC_I2C2_SCL_SELECT_INPUT_DAISY(1);&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;with&lt;/P&gt;&lt;P&gt;&lt;SPAN style="background-color: #f6f6f6;"&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;IOMUXC_I2C2_SCL_SELECT_INPUT = IOMUXC_I2C2_SCL_SELECT_INPUT_DAISY(0);&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;in the example&amp;nbsp;to adjust the pin mux to&amp;nbsp;UART2 pins?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 05 Feb 2018 10:50:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Pin-Config-vs-Pin-Mux/m-p/717579#M111523</guid>
      <dc:creator>demoniacmilk</dc:creator>
      <dc:date>2018-02-05T10:50:14Z</dc:date>
    </item>
    <item>
      <title>Re: Pin Config vs Pin Mux</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Pin-Config-vs-Pin-Mux/m-p/717580#M111524</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Lars&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;daisy functionality is described in 8.2.3.3 Daisy chain - multi pads driving same&lt;/P&gt;&lt;P&gt;module input pin i.MX7D Reference Manual &lt;/P&gt;&lt;P&gt;&lt;A class="jive-link-external-small" href="https://community.nxp.com/external-link.jspa?url=http%3A%2F%2Fcache.nxp.com%2Ffiles%2F32bit%2Fdoc%2Fref_manual%2FIMX7DRM.pdf" rel="nofollow" target="_blank"&gt;http://cache.nxp.com/files/32bit/doc/ref_manual/IMX7DRM.pdf&lt;/A&gt;&lt;BR /&gt;and used for some modules like uart. It is not used for i2c so seems its settings&lt;/P&gt;&lt;P&gt;can be changed.&lt;/P&gt;&lt;P&gt;**PAD_CTL_PAD iomux settings greatly depends on customer layout and usage,&lt;/P&gt;&lt;P&gt;so these settings should be adjusted by customer himself. As starting point one&lt;/P&gt;&lt;P&gt;can use default settings.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 06 Feb 2018 05:12:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Pin-Config-vs-Pin-Mux/m-p/717580#M111524</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2018-02-06T05:12:12Z</dc:date>
    </item>
  </channel>
</rss>