<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Differences between iMX7 Sabre Rev B and Rev D in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Differences-between-iMX7-Sabre-Rev-B-and-Rev-D/m-p/717314#M111470</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Based on what I read, am I right in assuming that for SD1 the only way to support SDR104 is to set it in the fuses?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 25 Oct 2017 14:45:23 GMT</pubDate>
    <dc:creator>brianpaiva</dc:creator>
    <dc:date>2017-10-25T14:45:23Z</dc:date>
    <item>
      <title>Differences between iMX7 Sabre Rev B and Rev D</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Differences-between-iMX7-Sabre-Rev-B-and-Rev-D/m-p/717312#M111468</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have an MCIMX7D-SABRE RevB (SCH-28590 Rev B), but the only schematic that I can find is for Rev D(SCH-28590 Rev D).&amp;nbsp; Are there any major differences between the two and is there a Rev B schematic available?&amp;nbsp; I'm trying to get support for SDR104 SD Cards, but can't get it to work in 1.8V mode.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 24 Oct 2017 14:34:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Differences-between-iMX7-Sabre-Rev-B-and-Rev-D/m-p/717312#M111468</guid>
      <dc:creator>brianpaiva</dc:creator>
      <dc:date>2017-10-24T14:34:53Z</dc:date>
    </item>
    <item>
      <title>Re: Differences between iMX7 Sabre Rev B and Rev D</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Differences-between-iMX7-Sabre-Rev-B-and-Rev-D/m-p/717313#M111469</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Brian,&lt;/P&gt;&lt;P&gt;all changes should be listed on the first page of the board schematic.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Jan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 25 Oct 2017 07:38:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Differences-between-iMX7-Sabre-Rev-B-and-Rev-D/m-p/717313#M111469</guid>
      <dc:creator>jan_spurek</dc:creator>
      <dc:date>2017-10-25T07:38:43Z</dc:date>
    </item>
    <item>
      <title>Re: Differences between iMX7 Sabre Rev B and Rev D</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Differences-between-iMX7-Sabre-Rev-B-and-Rev-D/m-p/717314#M111470</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Based on what I read, am I right in assuming that for SD1 the only way to support SDR104 is to set it in the fuses?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 25 Oct 2017 14:45:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Differences-between-iMX7-Sabre-Rev-B-and-Rev-D/m-p/717314#M111470</guid>
      <dc:creator>brianpaiva</dc:creator>
      <dc:date>2017-10-25T14:45:23Z</dc:date>
    </item>
    <item>
      <title>Re: Differences between iMX7 Sabre Rev B and Rev D</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Differences-between-iMX7-Sabre-Rev-B-and-Rev-D/m-p/717315#M111471</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&amp;nbsp; NVCC_SD1 supply voltage is provided by the PMIC on the i.MX7 SABRE &lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;design. This voltage is configured using SD_VSEL signal of the PMIC:&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;SD_VSEL is input from i.MX processor (GPIO1_IO08 on the SABRE) to select &lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;VCC_SD regulator voltage. So, SD1 supply voltage is programmable.&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&amp;nbsp;&amp;nbsp; IMX7 GPIO1_IO08 default state is GPIO port, input, pulled down, therefore&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;just after reset NVCC_SD1 is 3 V. Customers cannot change it for SD1 boot,&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;but can modify the voltage after boot in OS.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Yuri&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 26 Oct 2017 02:53:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Differences-between-iMX7-Sabre-Rev-B-and-Rev-D/m-p/717315#M111471</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2017-10-26T02:53:56Z</dc:date>
    </item>
  </channel>
</rss>