<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: iMX6DP/QP and eMMC HS200 mode in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/iMX6DP-QP-and-eMMC-HS200-mode/m-p/717244#M111452</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks! I didn't notice that a new reference manual was released.&lt;/P&gt;&lt;P&gt;I modified the driver to use HS200 and from my first test it was working (SDx_CLK was according to HS200) and the transfer rate from the eMMC also increased by 60%. But it's probably just "luck" that it works...&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 10 Apr 2018 06:32:21 GMT</pubDate>
    <dc:creator>JohnDoe1z</dc:creator>
    <dc:date>2018-04-10T06:32:21Z</dc:date>
    <item>
      <title>iMX6DP/QP and eMMC HS200 mode</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX6DP-QP-and-eMMC-HS200-mode/m-p/717242#M111450</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;the iMX6 DualPlus reference manual states that the uSDHC supports the MMC HS200 mode (section 68.1.2.1). However, the &lt;A href="http://git.freescale.com/git/cgit.cgi/imx/linux-imx.git/tree/drivers/mmc/host/sdhci-esdhc-imx.c?h=imx_4.9.11_1.0.0_ga"&gt;uSDHC driver coming with linux 4.9.11&amp;nbsp;&lt;/A&gt;does not advertise the HS200 mode for the DP/QP variants.&lt;/P&gt;&lt;P&gt;Is the HS200 mode supported by the iMX6 DP/QP and if so, why is the driver not reflecting that?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 09 Apr 2018 14:22:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX6DP-QP-and-eMMC-HS200-mode/m-p/717242#M111450</guid>
      <dc:creator>JohnDoe1z</dc:creator>
      <dc:date>2018-04-09T14:22:20Z</dc:date>
    </item>
    <item>
      <title>Re: iMX6DP/QP and eMMC HS200 mode</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX6DP-QP-and-eMMC-HS200-mode/m-p/717243#M111451</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi JohnDoe1z&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;it does not support HS200 mode and latest rev.1 Reference Manual (2017)&lt;/P&gt;&lt;P&gt;has not reference to HS200.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 09 Apr 2018 22:59:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX6DP-QP-and-eMMC-HS200-mode/m-p/717243#M111451</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2018-04-09T22:59:06Z</dc:date>
    </item>
    <item>
      <title>Re: iMX6DP/QP and eMMC HS200 mode</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX6DP-QP-and-eMMC-HS200-mode/m-p/717244#M111452</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks! I didn't notice that a new reference manual was released.&lt;/P&gt;&lt;P&gt;I modified the driver to use HS200 and from my first test it was working (SDx_CLK was according to HS200) and the transfer rate from the eMMC also increased by 60%. But it's probably just "luck" that it works...&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 10 Apr 2018 06:32:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX6DP-QP-and-eMMC-HS200-mode/m-p/717244#M111452</guid>
      <dc:creator>JohnDoe1z</dc:creator>
      <dc:date>2018-04-10T06:32:21Z</dc:date>
    </item>
  </channel>
</rss>