<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: USB power setting</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/USB-power-setting/m-p/716465#M111322</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Igor,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you for your quick response. I reviewed the Manual and was unable to find the current setting. Can you please point me to the correct source file that I could review?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Additionally, I'm hoping that there is a setting in the driver which will&amp;nbsp;allow the USB Host&amp;nbsp;to deny the request from&amp;nbsp;devices when they request additional current. (i.e. only allow max 100mA (default)).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can you please confirm that if I'm using USB1 in &lt;STRONG&gt;HOST mode only&lt;/STRONG&gt; then connecting the VBUS enable&amp;nbsp;to the USB_OTG1_PWR will allows the USB PHY to control the power (On/Off) to the device?&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/4263i340F5F907A93EA8E/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Santhosh&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 25 Oct 2017 14:37:54 GMT</pubDate>
    <dc:creator>srcoolz</dc:creator>
    <dc:date>2017-10-25T14:37:54Z</dc:date>
    <item>
      <title>USB power setting</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/USB-power-setting/m-p/716463#M111320</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am using the iMX6UL part and wanted to know how to set the USB current level. By default, USB Host provides 100mA @ 5V to begin and then after negotiations can provide upto 500mA. Is there a way in software (USB driver) to ensure that during negotiations the USB Host (iMX6UL) only allows upto 100mA and no more.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I understand that this is not USB 2.0 compliant - but in my system I'm unable to provide more than 0.5W of power to USB devices. We plan to use only USB memory stick as acceptable devices.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can you please help me with the setup or modifications needed to the USB driver?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Santhosh&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 25 Oct 2017 01:20:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/USB-power-setting/m-p/716463#M111320</guid>
      <dc:creator>srcoolz</dc:creator>
      <dc:date>2017-10-25T01:20:44Z</dc:date>
    </item>
    <item>
      <title>Re: USB power setting</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/USB-power-setting/m-p/716464#M111321</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&amp;nbsp; Santhosh&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;usb driver is described in&amp;nbsp; Chapter 39 CHIPIDEA USB Driver &lt;BR /&gt;attached Linux Manual and from sources seems driver supports only default 100mA setting.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 25 Oct 2017 03:02:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/USB-power-setting/m-p/716464#M111321</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2017-10-25T03:02:44Z</dc:date>
    </item>
    <item>
      <title>Re: USB power setting</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/USB-power-setting/m-p/716465#M111322</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Igor,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you for your quick response. I reviewed the Manual and was unable to find the current setting. Can you please point me to the correct source file that I could review?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Additionally, I'm hoping that there is a setting in the driver which will&amp;nbsp;allow the USB Host&amp;nbsp;to deny the request from&amp;nbsp;devices when they request additional current. (i.e. only allow max 100mA (default)).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can you please confirm that if I'm using USB1 in &lt;STRONG&gt;HOST mode only&lt;/STRONG&gt; then connecting the VBUS enable&amp;nbsp;to the USB_OTG1_PWR will allows the USB PHY to control the power (On/Off) to the device?&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/4263i340F5F907A93EA8E/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Santhosh&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 25 Oct 2017 14:37:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/USB-power-setting/m-p/716465#M111322</guid>
      <dc:creator>srcoolz</dc:creator>
      <dc:date>2017-10-25T14:37:54Z</dc:date>
    </item>
  </channel>
</rss>