<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: i.MX6 DMFC FIFO size</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6-DMFC-FIFO-size/m-p/715739#M111218</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Here is a misprint in the table you quoted. It means 128-bits lines.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Victor&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 13 Dec 2017 05:43:58 GMT</pubDate>
    <dc:creator>b36401</dc:creator>
    <dc:date>2017-12-13T05:43:58Z</dc:date>
    <item>
      <title>i.MX6 DMFC FIFO size</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6-DMFC-FIFO-size/m-p/715738#M111217</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have a question about DMFC FIFO size of i.MX6 IPU.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There is a description in reference manual, "The DMFC's write FIFO is built of 1024 entries of 128-bits each."&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/10271i250D85CCDB720752/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1. Does this FIFO size means 512 entry x 128bit(4words) instead of All(512x128 words) of dmfc_fifo_size_5c description?&lt;/P&gt;&lt;P&gt;2. Does FIFO&amp;nbsp;separate two planes as 512 entry x 128bit fro 1024 x128bit?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Sugiyama&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 12 Dec 2017 09:39:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6-DMFC-FIFO-size/m-p/715738#M111217</guid>
      <dc:creator>sugiyamatoshihi</dc:creator>
      <dc:date>2017-12-12T09:39:58Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX6 DMFC FIFO size</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6-DMFC-FIFO-size/m-p/715739#M111218</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Here is a misprint in the table you quoted. It means 128-bits lines.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Victor&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 13 Dec 2017 05:43:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6-DMFC-FIFO-size/m-p/715739#M111218</guid>
      <dc:creator>b36401</dc:creator>
      <dc:date>2017-12-13T05:43:58Z</dc:date>
    </item>
  </channel>
</rss>