<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: viv_samples in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/viv-samples/m-p/715692#M111203</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi &lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/igorpadykov"&gt;igorpadykov&lt;/A&gt;‌&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I went through above link and it has extracted Samples residing inside fsl-gpu-sdk-1.1 &amp;amp; fsl-gpu-sdk-2.2.2 but don't see source code of tiger demo (also no source code of vv_launcher demo.&lt;/P&gt;&lt;P&gt;The thing is i need this is to understand how it is launch so as it is not hiding background. I have use-case where I have to show b.g. as it is while running any GLES2.0 demo.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;While running tiger demo which comes as prebuilt in imx-gpu-viv-6.2.4.p4.0-aarch64.bin render tiger on top of QT5 background very well. But when I run any of the GLES2.0 demos, it hides b.g. QT GUI. I went through many post to do blending but without success.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you have idea where i can get source code of tiger demo, I can compare with GLES2.0 based my demo and do needful to achieve usecase.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;--&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Hitesh&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 27 Nov 2019 12:31:40 GMT</pubDate>
    <dc:creator>hiteshviradiya</dc:creator>
    <dc:date>2019-11-27T12:31:40Z</dc:date>
    <item>
      <title>viv_samples</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/viv-samples/m-p/715690#M111201</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;yocto 3.14.52 for imx6q. how can i get the demos source code of the viv_samples？&lt;/P&gt;&lt;P&gt;怎么能拿到/opt/viv_samples下的源码文件呢？不要可执行的。&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 12 Dec 2017 07:17:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/viv-samples/m-p/715690#M111201</guid>
      <dc:creator>tukenan</dc:creator>
      <dc:date>2017-12-12T07:17:44Z</dc:date>
    </item>
    <item>
      <title>Re: viv_samples</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/viv-samples/m-p/715691#M111202</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;please look at&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://layers.openembedded.org/layerindex/recipe/26744/" title="https://layers.openembedded.org/layerindex/recipe/26744/"&gt;OpenEmbedded Layer Index - fsl-gpu-sdk&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;and Vivante VTK on&lt;/P&gt;&lt;P&gt;&lt;A class="jive-link-external-small" href="https://community.nxp.com/external-link.jspa?url=http%3A%2F%2Fwww.nxp.com%2Fproducts%2Fsoftware-and-tools%2Fsoftware-development-tools%2Fi.mx-software-and-tools%2Fi.mx-6series-i.mx-7series-software-and-development-tool-resources%3AIMX_SW" rel="nofollow" target="_blank"&gt;http://www.nxp.com/products/software-and-tools/software-development-tools/i.mx-software-and-tools/i.mx-6series-i.mx-7series-software-and-development-tool-resources:IMX_SW&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 12 Dec 2017 10:29:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/viv-samples/m-p/715691#M111202</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2017-12-12T10:29:22Z</dc:date>
    </item>
    <item>
      <title>Re: viv_samples</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/viv-samples/m-p/715692#M111203</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi &lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/igorpadykov"&gt;igorpadykov&lt;/A&gt;‌&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I went through above link and it has extracted Samples residing inside fsl-gpu-sdk-1.1 &amp;amp; fsl-gpu-sdk-2.2.2 but don't see source code of tiger demo (also no source code of vv_launcher demo.&lt;/P&gt;&lt;P&gt;The thing is i need this is to understand how it is launch so as it is not hiding background. I have use-case where I have to show b.g. as it is while running any GLES2.0 demo.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;While running tiger demo which comes as prebuilt in imx-gpu-viv-6.2.4.p4.0-aarch64.bin render tiger on top of QT5 background very well. But when I run any of the GLES2.0 demos, it hides b.g. QT GUI. I went through many post to do blending but without success.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you have idea where i can get source code of tiger demo, I can compare with GLES2.0 based my demo and do needful to achieve usecase.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;--&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Hitesh&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 27 Nov 2019 12:31:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/viv-samples/m-p/715692#M111203</guid>
      <dc:creator>hiteshviradiya</dc:creator>
      <dc:date>2019-11-27T12:31:40Z</dc:date>
    </item>
  </channel>
</rss>