<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 i.MX6ULL Linux Display Drivers</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6ULL-Linux-Display-Drivers/m-p/715109#M111144</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;My customer is trying to find which Linux display drivers are available, and also what LCD Digital Drivers are supported with any existing Linux drivers.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Ideally something similar to the Himax HX8238-D see attached, we would like to use in the 8bit data/ SPI control mode.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 27 Sep 2017 21:45:45 GMT</pubDate>
    <dc:creator>khollar</dc:creator>
    <dc:date>2017-09-27T21:45:45Z</dc:date>
    <item>
      <title>i.MX6ULL Linux Display Drivers</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6ULL-Linux-Display-Drivers/m-p/715109#M111144</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;My customer is trying to find which Linux display drivers are available, and also what LCD Digital Drivers are supported with any existing Linux drivers.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Ideally something similar to the Himax HX8238-D see attached, we would like to use in the 8bit data/ SPI control mode.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 27 Sep 2017 21:45:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6ULL-Linux-Display-Drivers/m-p/715109#M111144</guid>
      <dc:creator>khollar</dc:creator>
      <dc:date>2017-09-27T21:45:45Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX6ULL Linux Display Drivers</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6ULL-Linux-Display-Drivers/m-p/715110#M111145</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;The default BSP Supports SEIKO WVGA panel. For i.MX 6UltraLite, i.MX 6ULL and i.MX 7Dual SABRE-SD, it supports Embest LCD8000-43T LCD panel.The LCD interface driver supports the Samsung LMS430xx 4.3" WQVGA LCD panel.&lt;/P&gt;&lt;P&gt;mxc_lcdif.c Display Driver for CLAA-WVGA and SEIKO-WVGA LCD support.Here if you want to use other LCD, you can connect and porting the screen driver to your board.&lt;/P&gt;&lt;P&gt;All the function and BSP Supported Features you can see the documents i.MX_Linux_Release_Notes.pdf and i.MX_Linux_Reference_Manual.pdf.&lt;BR /&gt;Have a great day,&lt;BR /&gt; Rita&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 29 Sep 2017 02:18:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6ULL-Linux-Display-Drivers/m-p/715110#M111145</guid>
      <dc:creator>Rita_Wang</dc:creator>
      <dc:date>2017-09-29T02:18:25Z</dc:date>
    </item>
  </channel>
</rss>