<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: FlexCAN on Android 7.1.1 in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/FlexCAN-on-Android-7-1-1/m-p/714984#M111131</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Aaron&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;sabre ai image will not work on sabre sd board as these two boards are different.&lt;/P&gt;&lt;P&gt;One can check sabre ai dts for can records and make similar changes to sabre sd file.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 06 Sep 2017 23:21:37 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2017-09-06T23:21:37Z</dc:date>
    <item>
      <title>FlexCAN on Android 7.1.1</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/FlexCAN-on-Android-7-1-1/m-p/714979#M111126</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello all,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;How do I add the Freescale FlexCAN driver (&lt;A href="https://community.nxp.com/docs/DOC-1437"&gt;All Boards FlexCAN&lt;/A&gt;&amp;nbsp;) to the latest android kernel from freescale (n7.1.1_1.0.0-ga)?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for your help,&lt;/P&gt;&lt;P&gt;Aaron&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 04 Sep 2017 14:46:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/FlexCAN-on-Android-7-1-1/m-p/714979#M111126</guid>
      <dc:creator>tommos23</dc:creator>
      <dc:date>2017-09-04T14:46:52Z</dc:date>
    </item>
    <item>
      <title>Re: FlexCAN on Android 7.1.1</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/FlexCAN-on-Android-7-1-1/m-p/714980#M111127</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Aaron&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;seems android flexcan usage may be similar to previous versions, so one can&lt;/P&gt;&lt;P&gt;look at efforts described on&lt;/P&gt;&lt;P&gt;&lt;A _jive_internal="true" data-containerid="2004" data-containertype="14" data-objectid="333623" data-objecttype="1" href="https://community.nxp.com/thread/333623"&gt;https://community.nxp.com/thread/333623&lt;/A&gt;&lt;BR /&gt;&lt;A class="jive-link-external-small" href="https://community.nxp.com/external-link.jspa?url=https%3A%2F%2Fgithub.com%2Fryangithub%2Fsunxi-can-driver" rel="nofollow" target="_blank"&gt;https://github.com/ryangithub/sunxi-can-driver&lt;/A&gt;&lt;BR /&gt;&lt;A href="https://www.technexion.com/products/system-on-modules/edm/edm-modules/detail/EDM1-CF-IMX6"&gt;https://www.technexion.com/products/system-on-modules/edm/edm-modules/detail/EDM1-CF-IMX6 &lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 04 Sep 2017 23:23:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/FlexCAN-on-Android-7-1-1/m-p/714980#M111127</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2017-09-04T23:23:07Z</dc:date>
    </item>
    <item>
      <title>Re: FlexCAN on Android 7.1.1</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/FlexCAN-on-Android-7-1-1/m-p/714981#M111128</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Igor,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for the reply this will come in very handy in the future but the root problem I am having is that 'can0' or 'can1' do not appear in the list of devices when typing 'ifconfig -all'.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/29325iE7B87C2301038D21/image-size/large?v=v2&amp;amp;px=999" title="ipLinkSet.PNG" alt="ipLinkSet.PNG" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;How do I add the can devices to the Linux kernel in the freescale Android 7.1.1 release?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Aaron&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 05 Sep 2017 08:07:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/FlexCAN-on-Android-7-1-1/m-p/714981#M111128</guid>
      <dc:creator>tommos23</dc:creator>
      <dc:date>2017-09-05T08:07:11Z</dc:date>
    </item>
    <item>
      <title>Re: FlexCAN on Android 7.1.1</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/FlexCAN-on-Android-7-1-1/m-p/714982#M111129</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Aaron&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;sabresd board does not support flexcan, please build image for&lt;/P&gt;&lt;P&gt;sabre ai board which supports flexcan, refer to sect.37.2.4 Linux Menu Configuration&lt;/P&gt;&lt;P&gt;Options attached Linux Manual.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 05 Sep 2017 10:16:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/FlexCAN-on-Android-7-1-1/m-p/714982#M111129</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2017-09-05T10:16:51Z</dc:date>
    </item>
    <item>
      <title>Re: FlexCAN on Android 7.1.1</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/FlexCAN-on-Android-7-1-1/m-p/714983#M111130</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Igor,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I built the image for saber ai (sabreauto_6q) however this does not&amp;nbsp;appear to work on the sabreSD board.&lt;/P&gt;&lt;P&gt;I am using&amp;nbsp;mfgtools to load the image into emmc (mfgtool2-android-mx6dl-sabresd-emmc.vbs). Did I use the correct configuration?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Aaron&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 06 Sep 2017 14:41:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/FlexCAN-on-Android-7-1-1/m-p/714983#M111130</guid>
      <dc:creator>tommos23</dc:creator>
      <dc:date>2017-09-06T14:41:15Z</dc:date>
    </item>
    <item>
      <title>Re: FlexCAN on Android 7.1.1</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/FlexCAN-on-Android-7-1-1/m-p/714984#M111131</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Aaron&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;sabre ai image will not work on sabre sd board as these two boards are different.&lt;/P&gt;&lt;P&gt;One can check sabre ai dts for can records and make similar changes to sabre sd file.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 06 Sep 2017 23:21:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/FlexCAN-on-Android-7-1-1/m-p/714984#M111131</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2017-09-06T23:21:37Z</dc:date>
    </item>
  </channel>
</rss>