<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: cross compiling a c program for imx6</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/cross-compiling-a-c-program-for-imx6/m-p/714686#M111092</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello sameerarvikar,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This error may be related to the libraries not being found when cross-compiling. One alternative would be looking for the libraries on your gcc location and adding them to LIBRARY_PATH.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I would recommend looking at the following thread where they set a flag to point to where the target sysroot is, which allows the cross compiler to find the libraries:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A class="jive-link-thread-small" data-containerid="2004" data-containertype="14" data-objectid="394804" data-objecttype="1" href="https://community.nxp.com/thread/394804"&gt;https://community.nxp.com/thread/394804&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 05 Oct 2017 15:11:52 GMT</pubDate>
    <dc:creator>gusarambula</dc:creator>
    <dc:date>2017-10-05T15:11:52Z</dc:date>
    <item>
      <title>cross compiling a c program for imx6</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/cross-compiling-a-c-program-for-imx6/m-p/714685#M111091</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I am trying to cross compile following c (tcp socket server)program for imx6&lt;/P&gt;&lt;P&gt;using following command&lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;arm-poky-linux-gnueabi-gcc tcpserver.c --sysroot=/opt/fsl-imx-x11/4.1.15-2.0.1/sysroots/cortexa9hf-neon-poky-linux-gnueabi/usr/lib -o server_tcp -I/opt/fsl-imx-x11/4.1.15-2.0.1/sysroots/cortexa9hf-neon-poky-linux-gnueabi/usr/include&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;I have include -I option cause error was coming stdio.h&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Now error is coming&lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;/opt/fsl-imx-x11/4.1.15-2.0.1/sysroots/cortexa9hf-neon-poky-linux-gnueabi/usr/include/gnu/stubs.h:7:29: fatal error: gnu/stubs-soft.h: No such file or directory&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;so i edited stubs.h&lt;/P&gt;&lt;P&gt;so it won't use stubs-soft.h&lt;/P&gt;&lt;P&gt;Now following error is coming&lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;/opt/fsl-imx-x11/4.1.15-2.0.1/sysroots/x86_64-pokysdk-linux/usr/libexec/arm-poky-linux-gnueabi/gcc/arm-poky-linux-gnueabi/5.3.0/real-ld: cannot find crt1.o: No such file or directory&lt;BR /&gt;/opt/fsl-imx-x11/4.1.15-2.0.1/sysroots/x86_64-pokysdk-linux/usr/libexec/arm-poky-linux-gnueabi/gcc/arm-poky-linux-gnueabi/5.3.0/real-ld: cannot find crti.o: No such file or directory&lt;BR /&gt;/opt/fsl-imx-x11/4.1.15-2.0.1/sysroots/x86_64-pokysdk-linux/usr/libexec/arm-poky-linux-gnueabi/gcc/arm-poky-linux-gnueabi/5.3.0/real-ld: cannot find crtbegin.o: No such file or directory&lt;BR /&gt;/opt/fsl-imx-x11/4.1.15-2.0.1/sysroots/x86_64-pokysdk-linux/usr/libexec/arm-poky-linux-gnueabi/gcc/arm-poky-linux-gnueabi/5.3.0/real-ld: cannot find -lgcc&lt;BR /&gt;/opt/fsl-imx-x11/4.1.15-2.0.1/sysroots/x86_64-pokysdk-linux/usr/libexec/arm-poky-linux-gnueabi/gcc/arm-poky-linux-gnueabi/5.3.0/real-ld: cannot find -lgcc_s&lt;BR /&gt;/opt/fsl-imx-x11/4.1.15-2.0.1/sysroots/x86_64-pokysdk-linux/usr/libexec/arm-poky-linux-gnueabi/gcc/arm-poky-linux-gnueabi/5.3.0/real-ld: cannot find -lc&lt;BR /&gt;/opt/fsl-imx-x11/4.1.15-2.0.1/sysroots/x86_64-pokysdk-linux/usr/libexec/arm-poky-linux-gnueabi/gcc/arm-poky-linux-gnueabi/5.3.0/real-ld: cannot find -lgcc&lt;BR /&gt;/opt/fsl-imx-x11/4.1.15-2.0.1/sysroots/x86_64-pokysdk-linux/usr/libexec/arm-poky-linux-gnueabi/gcc/arm-poky-linux-gnueabi/5.3.0/real-ld: cannot find -lgcc_s&lt;BR /&gt;/opt/fsl-imx-x11/4.1.15-2.0.1/sysroots/x86_64-pokysdk-linux/usr/libexec/arm-poky-linux-gnueabi/gcc/arm-poky-linux-gnueabi/5.3.0/real-ld: cannot find crtend.o: No such file or directory&lt;BR /&gt;/opt/fsl-imx-x11/4.1.15-2.0.1/sysroots/x86_64-pokysdk-linux/usr/libexec/arm-poky-linux-gnueabi/gcc/arm-poky-linux-gnueabi/5.3.0/real-ld: cannot find crtn.o: No such file or directory&lt;BR /&gt;collect2: error: ld returned 1 exit status&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 15px;"&gt;&lt;STRONG&gt;how to solve the issue ,the program is compiling and running without problem in ubuntu(on pc)&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;tcpserver.c&lt;/P&gt;&lt;P&gt;/****************** SERVER CODE ****************/&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;#include &amp;lt;stdio.h&amp;gt;&lt;BR /&gt;#include &amp;lt;sys/socket.h&amp;gt;&lt;BR /&gt;#include &amp;lt;netinet/in.h&amp;gt;&lt;BR /&gt;#include &amp;lt;string.h&amp;gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;int main(){&lt;BR /&gt;&amp;nbsp; int welcomeSocket, newSocket;&lt;BR /&gt;&amp;nbsp; char buffer[1024];&lt;BR /&gt;&amp;nbsp; struct sockaddr_in serverAddr;&lt;BR /&gt;&amp;nbsp; struct sockaddr_storage serverStorage;&lt;BR /&gt;&amp;nbsp; socklen_t addr_size;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; /*---- Create the socket. The three arguments are: ----*/&lt;BR /&gt;&amp;nbsp; /* 1) Internet domain 2) Stream socket 3) Default protocol (TCP in this case) */&lt;BR /&gt;&amp;nbsp; welcomeSocket = socket(PF_INET, SOCK_STREAM, 0);&lt;BR /&gt;&amp;nbsp; &lt;BR /&gt;&amp;nbsp; /*---- Configure settings of the server address struct ----*/&lt;BR /&gt;&amp;nbsp; /* Address family = Internet */&lt;BR /&gt;&amp;nbsp; serverAddr.sin_family = AF_INET;&lt;BR /&gt;&amp;nbsp; /* Set port number, using htons function to use proper byte order */&lt;BR /&gt;&amp;nbsp; serverAddr.sin_port = htons(7891);&lt;BR /&gt;&amp;nbsp; /* Set IP address to localhost */&lt;BR /&gt;&amp;nbsp; serverAddr.sin_addr.s_addr = inet_addr("127.0.0.1");&lt;BR /&gt;&amp;nbsp; /* Set all bits of the padding field to 0 */&lt;BR /&gt;&amp;nbsp; memset(serverAddr.sin_zero, '\0', sizeof serverAddr.sin_zero); &amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; /*---- Bind the address struct to the socket ----*/&lt;BR /&gt;&amp;nbsp; bind(welcomeSocket, (struct sockaddr *) &amp;amp;serverAddr, sizeof(serverAddr));&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; /*---- Listen on the socket, with 5 max connection requests queued ----*/&lt;BR /&gt;&amp;nbsp; if(listen(welcomeSocket,5)==0)&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; printf("Listening\n");&lt;BR /&gt;&amp;nbsp; else&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; printf("Error\n");&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; /*---- Accept call creates a new socket for the incoming connection ----*/&lt;BR /&gt;&amp;nbsp; addr_size = sizeof serverStorage;&lt;BR /&gt;&amp;nbsp; &lt;BR /&gt;&amp;nbsp; int n = 0, k;&lt;BR /&gt;&amp;nbsp; char recvBuff[1024];&lt;BR /&gt;&amp;nbsp;while(1)&lt;BR /&gt;&amp;nbsp;{&lt;BR /&gt;&amp;nbsp; newSocket = accept(welcomeSocket, (struct sockaddr *) &amp;amp;serverStorage, &amp;amp;addr_size);&lt;BR /&gt;&amp;nbsp;/*---- Send message to the socket of the incoming connection ----*/&lt;BR /&gt;&amp;nbsp; strcpy(buffer,"Hello World\n");&lt;BR /&gt;&amp;nbsp; send(newSocket,buffer,13,0);&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;n = recv(newSocket, recvBuff, 1023, 0);&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; printf("Recd: %d bytes\n",n);&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; printf("Data received: %s",recvBuff); &lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* printf("recvbuff --&amp;gt; %s&amp;nbsp; \n",recvBuff); */&lt;BR /&gt;&amp;nbsp; /*&amp;nbsp; for (k=0; k&amp;lt;16; ++k) { printf("%d: 0x%02s, ", k, recvBuff[k]); }&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; sleep(1);*/&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;printf("\n");&lt;BR /&gt;&amp;nbsp;}&lt;BR /&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; return 0;&lt;BR /&gt;}&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 27 Sep 2017 10:32:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/cross-compiling-a-c-program-for-imx6/m-p/714685#M111091</guid>
      <dc:creator>sameerarvikar</dc:creator>
      <dc:date>2017-09-27T10:32:37Z</dc:date>
    </item>
    <item>
      <title>Re: cross compiling a c program for imx6</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/cross-compiling-a-c-program-for-imx6/m-p/714686#M111092</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello sameerarvikar,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This error may be related to the libraries not being found when cross-compiling. One alternative would be looking for the libraries on your gcc location and adding them to LIBRARY_PATH.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I would recommend looking at the following thread where they set a flag to point to where the target sysroot is, which allows the cross compiler to find the libraries:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A class="jive-link-thread-small" data-containerid="2004" data-containertype="14" data-objectid="394804" data-objecttype="1" href="https://community.nxp.com/thread/394804"&gt;https://community.nxp.com/thread/394804&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 05 Oct 2017 15:11:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/cross-compiling-a-c-program-for-imx6/m-p/714686#M111092</guid>
      <dc:creator>gusarambula</dc:creator>
      <dc:date>2017-10-05T15:11:52Z</dc:date>
    </item>
  </channel>
</rss>