<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Unexpected SPI frequency variation</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Unexpected-SPI-frequency-variation/m-p/714358#M111035</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Deven,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;which BSP/kernel are you using?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Carlos&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 26 Sep 2017 20:02:37 GMT</pubDate>
    <dc:creator>Carlos_Musich</dc:creator>
    <dc:date>2017-09-26T20:02:37Z</dc:date>
    <item>
      <title>Unexpected SPI frequency variation</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Unexpected-SPI-frequency-variation/m-p/714357#M111034</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am working in imx7d sabresd. Right now I am testing SPI which is available in mikrobus with spitest application (link: &lt;A class="link-titled" href="https://raw.githubusercontent.com/raspberrypi/linux/rpi-3.10.y/Documentation/spi/spidev_test.c" title="https://raw.githubusercontent.com/raspberrypi/linux/rpi-3.10.y/Documentation/spi/spidev_test.c"&gt;https://raw.githubusercontent.com/raspberrypi/linux/rpi-3.10.y/Documentation/spi/spidev_test.c&lt;/A&gt;).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am changing frequency (from application) so mostly I am getting nearby clock value(like for 25MHz output frequency is 20MHz), that is ok because it is using divider.&lt;/P&gt;&lt;P&gt;But when I am giving 3MHz,4MHz,8MHz and 9MHz I am getting very low frequency(below 1MHz), and when I am giving 2MHz it is reflecting as same 2Mhz. Why it is like that?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 04 Sep 2017 10:43:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Unexpected-SPI-frequency-variation/m-p/714357#M111034</guid>
      <dc:creator>deven_solanki</dc:creator>
      <dc:date>2017-09-04T10:43:38Z</dc:date>
    </item>
    <item>
      <title>Re: Unexpected SPI frequency variation</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Unexpected-SPI-frequency-variation/m-p/714358#M111035</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Deven,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;which BSP/kernel are you using?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Carlos&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 26 Sep 2017 20:02:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Unexpected-SPI-frequency-variation/m-p/714358#M111035</guid>
      <dc:creator>Carlos_Musich</dc:creator>
      <dc:date>2017-09-26T20:02:37Z</dc:date>
    </item>
  </channel>
</rss>