<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: i.MX6ULL USB_OTG2 ROM loader</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6ULL-USB-OTG2-ROM-loader/m-p/714167#M110994</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Igor, thank you for this answer.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;According to the Reference Manual sect&amp;nbsp;8.9.1:&lt;/P&gt;&lt;P&gt;"The ROM supports the USB OTG port for boot purposes. The other USB ports on the chip are not supported for boot purposes."&lt;/P&gt;&lt;P&gt;I thought all the OTG ports are available for boot purposes.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 27 Sep 2017 06:56:04 GMT</pubDate>
    <dc:creator>chris321</dc:creator>
    <dc:date>2017-09-27T06:56:04Z</dc:date>
    <item>
      <title>i.MX6ULL USB_OTG2 ROM loader</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6ULL-USB-OTG2-ROM-loader/m-p/714165#M110992</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;according to the i.mx6ULL reference manual it is possible to use both USB OTG ports for ROM loading&amp;nbsp;purposes.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is the USB_OTG_ID pin&amp;nbsp;analyzed by the ROM?&lt;/P&gt;&lt;P&gt;I want to use the USB_OTG2 port for manufacturing a custom board and after that it should be in host mode.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I plan to use the following pads for the muxable USB signals:&lt;/P&gt;&lt;P&gt;usb_otg2_id --&amp;gt;GPIO1_IO05&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;usb_otg2_oc --&amp;gt; SD1_DATA2&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;usb_otg2_pwr --&amp;gt;SD1_DATA1&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I have a reference kit (compute module + base board) on my desk.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Is it possible to force the ROM loader to use the USB_OTG2&amp;nbsp;interface somehow?&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 26 Sep 2017 15:03:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6ULL-USB-OTG2-ROM-loader/m-p/714165#M110992</guid>
      <dc:creator>chris321</dc:creator>
      <dc:date>2017-09-26T15:03:06Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX6ULL USB_OTG2 ROM loader</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6ULL-USB-OTG2-ROM-loader/m-p/714166#M110993</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi chris321&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;USB_OTG_ID pin is not analyzed by the ROM. Also only USB_OTG1&lt;/P&gt;&lt;P&gt;is used by ROM according to i.MX6ULL Reference Manual sect.8.2.4 Serial Downloader&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://www.nxp.com/docs/en/reference-manual/IMX6ULLRM.pdf" title="https://www.nxp.com/docs/en/reference-manual/IMX6ULLRM.pdf"&gt;https://www.nxp.com/docs/en/reference-manual/IMX6ULLRM.pdf&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 26 Sep 2017 23:13:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6ULL-USB-OTG2-ROM-loader/m-p/714166#M110993</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2017-09-26T23:13:12Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX6ULL USB_OTG2 ROM loader</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6ULL-USB-OTG2-ROM-loader/m-p/714167#M110994</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Igor, thank you for this answer.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;According to the Reference Manual sect&amp;nbsp;8.9.1:&lt;/P&gt;&lt;P&gt;"The ROM supports the USB OTG port for boot purposes. The other USB ports on the chip are not supported for boot purposes."&lt;/P&gt;&lt;P&gt;I thought all the OTG ports are available for boot purposes.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 27 Sep 2017 06:56:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6ULL-USB-OTG2-ROM-loader/m-p/714167#M110994</guid>
      <dc:creator>chris321</dc:creator>
      <dc:date>2017-09-27T06:56:04Z</dc:date>
    </item>
  </channel>
</rss>