<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processorsのトピックrepo init command failing.</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/repo-init-command-failing/m-p/714029#M110980</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear All,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am following the "Freescale_Yocto_Project_User's_Guide.pdf" to do the setup of i.mx6 yocto build environment.&lt;/P&gt;&lt;P&gt;And when I run&lt;STRONG&gt; repo init &lt;/STRONG&gt;it is failing. Please find attached img.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please help!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 26 Sep 2017 15:28:13 GMT</pubDate>
    <dc:creator>indrajitkumar</dc:creator>
    <dc:date>2017-09-26T15:28:13Z</dc:date>
    <item>
      <title>repo init command failing.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/repo-init-command-failing/m-p/714029#M110980</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear All,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am following the "Freescale_Yocto_Project_User's_Guide.pdf" to do the setup of i.mx6 yocto build environment.&lt;/P&gt;&lt;P&gt;And when I run&lt;STRONG&gt; repo init &lt;/STRONG&gt;it is failing. Please find attached img.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please help!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 26 Sep 2017 15:28:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/repo-init-command-failing/m-p/714029#M110980</guid>
      <dc:creator>indrajitkumar</dc:creator>
      <dc:date>2017-09-26T15:28:13Z</dc:date>
    </item>
    <item>
      <title>Re: repo init command failing.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/repo-init-command-failing/m-p/714030#M110981</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Indrajit,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When 'repo init' process is completed, the source code is checked out into the directory &amp;lt;BSP-Directory&amp;gt;/sources. A successful initialization will end with a message stating that Repo is initialized in your working directory. Your client directory should contain a hidden .repo directory where files such as the manifest will be kept.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;First you may update and upgrade your host machine. If errors occur during repo initialization, try deleting the .repo directory and running the repo initialization command again.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;If the problems persists verify that you have internet connection and you may contact your system administrator because if you are using firewalls or porxy server this may avoid conenction to repo.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Regards,&lt;BR /&gt;Carlos&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 26 Sep 2017 16:53:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/repo-init-command-failing/m-p/714030#M110981</guid>
      <dc:creator>Carlos_Musich</dc:creator>
      <dc:date>2017-09-26T16:53:04Z</dc:date>
    </item>
    <item>
      <title>Re: repo init command failing.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/repo-init-command-failing/m-p/714031#M110982</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Carlos,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you very much for the quick reply.&lt;/P&gt;&lt;P&gt;Fortunately, &lt;STRONG&gt;repo init&lt;/STRONG&gt; command started working after doing the changes recommended by you.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But now, when I am trying &lt;STRONG&gt;repo sync, &lt;/STRONG&gt;it is not working. Please check the images.&lt;/P&gt;&lt;P&gt;I think there is no problem with internet connection and access rights on my system.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/48424i1CF95FD67EC6BF61/image-size/large?v=v2&amp;amp;px=999" title="repo_sync_error1.png" alt="repo_sync_error1.png" /&gt;&lt;/span&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/48484iD6351402C71A4932/image-size/large?v=v2&amp;amp;px=999" title="repo_sync_error.png" alt="repo_sync_error.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 27 Sep 2017 15:36:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/repo-init-command-failing/m-p/714031#M110982</guid>
      <dc:creator>indrajitkumar</dc:creator>
      <dc:date>2017-09-27T15:36:34Z</dc:date>
    </item>
    <item>
      <title>Re: repo init command failing.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/repo-init-command-failing/m-p/714032#M110983</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Indrajit,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For one or the other reason the GIT server is sometimes not reachable, but you still have the option to download the source code from &lt;A class="link-titled" href="http://git.freescale.com/git/" title="http://git.freescale.com/git/"&gt;Freescale Public GIT&lt;/A&gt; and then build it. If you have the need for various builds based on the same release, then it's useful to download all sources one time and base the following builds then on (a copy of) the local sources:&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;$ bitbake -c fetchall target&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In &lt;A class="link-titled" href="http://www.yoctoproject.org/docs/2.0/dev-manual/dev-manual.html" title="http://www.yoctoproject.org/docs/2.0/dev-manual/dev-manual.html"&gt;Yocto Project Development Manual&lt;/A&gt; in chapter 5.15 you find some more information.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Regards,&lt;BR /&gt;Carlos&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 28 Sep 2017 14:28:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/repo-init-command-failing/m-p/714032#M110983</guid>
      <dc:creator>Carlos_Musich</dc:creator>
      <dc:date>2017-09-28T14:28:26Z</dc:date>
    </item>
    <item>
      <title>Re: repo init command failing.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/repo-init-command-failing/m-p/714033#M110984</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks Carlos!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I will check your points.&lt;/P&gt;&lt;P&gt;Thank you very much :smileyhappy:&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 29 Sep 2017 08:03:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/repo-init-command-failing/m-p/714033#M110984</guid>
      <dc:creator>indrajitkumar</dc:creator>
      <dc:date>2017-09-29T08:03:26Z</dc:date>
    </item>
  </channel>
</rss>