<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: upgrade yocto kernel to support  to have missing kernel configuration option</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/upgrade-yocto-kernel-to-support-to-have-missing-kernel/m-p/710658#M110510</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Pehen Azam,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I would make sure that the driver is compatible with the 4.1.15 Kernel. I’m not familiar with this driver but the driver documentation should clarify which kernel versions are compatible. Depending on this you may need to switch kernel versions, but it would depend on the driver.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It looks like the driver is not available in a git, so you would need to add it manually to your linux distribution (either using yocto or manually). Some third parties do provide layers that are easily portable, or sometimes the drivers get ported to open source layers so you may also want to look for the driver on the yocto proyect layers.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 24 Oct 2017 16:47:44 GMT</pubDate>
    <dc:creator>gusarambula</dc:creator>
    <dc:date>2017-10-24T16:47:44Z</dc:date>
    <item>
      <title>upgrade yocto kernel to support  to have missing kernel configuration option</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/upgrade-yocto-kernel-to-support-to-have-missing-kernel/m-p/710657#M110509</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="background-color: #ffffff;"&gt;I am using&amp;nbsp;imx6p solo and&amp;nbsp;I'd like to add&lt;A href="http://www.ti.com/tool/OPT3001SW-LINUX"&gt; OPT3001 Digital Ambient Light Sensor &lt;/A&gt;to my linux kernel. However, kernel configuration option&lt;/SPAN&gt;s (Symbol: OPT3001 [=y]) is missing in the kernel that we are using. here is "uname -a"&lt;/P&gt;&lt;P&gt;&lt;SPAN style="background-color: #ffffff;"&gt;Linux acompany 4.1.15-1.2.0+g7d6134 #1 SMP PREEMPT Wed Oct 18 15:25:22 CEST 2017 armv7l GNU/Linux&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="background-color: #ffffff;"&gt;How I can upgrade kernel in yocto to support it? if not possible why? and how I can port&amp;nbsp; "&lt;/SPAN&gt;drivers/iio/light/opt3001.c" to our kernel?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="background-color: #ffffff;"&gt;Thanks&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 19 Oct 2017 12:07:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/upgrade-yocto-kernel-to-support-to-have-missing-kernel/m-p/710657#M110509</guid>
      <dc:creator>pehenazam</dc:creator>
      <dc:date>2017-10-19T12:07:10Z</dc:date>
    </item>
    <item>
      <title>Re: upgrade yocto kernel to support  to have missing kernel configuration option</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/upgrade-yocto-kernel-to-support-to-have-missing-kernel/m-p/710658#M110510</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Pehen Azam,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I would make sure that the driver is compatible with the 4.1.15 Kernel. I’m not familiar with this driver but the driver documentation should clarify which kernel versions are compatible. Depending on this you may need to switch kernel versions, but it would depend on the driver.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It looks like the driver is not available in a git, so you would need to add it manually to your linux distribution (either using yocto or manually). Some third parties do provide layers that are easily portable, or sometimes the drivers get ported to open source layers so you may also want to look for the driver on the yocto proyect layers.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 24 Oct 2017 16:47:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/upgrade-yocto-kernel-to-support-to-have-missing-kernel/m-p/710658#M110510</guid>
      <dc:creator>gusarambula</dc:creator>
      <dc:date>2017-10-24T16:47:44Z</dc:date>
    </item>
  </channel>
</rss>