<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processorsのトピックi.MX6UL u-boot doesn't recognize eMMC 5.1</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6UL-u-boot-doesn-t-recognize-eMMC-5-1/m-p/710321#M110448</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;on our custom board with i.MX6UL and eMMC 5.1, the bootloader doesn't recognize the eMMC.&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;The bootloader is loaded in serial download mode with the imx_usb_loader tool.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In uboot the following answers are shown:&lt;/P&gt;&lt;P&gt;mmc info =&amp;gt; no card present&lt;/P&gt;&lt;P&gt;mmc dev 1 =&amp;gt; Card did not respond to voltage select&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The eMMC schematic is the same as in i.MX6UL EVK.&lt;/P&gt;&lt;P&gt;The u-boot is made with fsl-arm-yocto-bsp (mx6ul_14x14_evk).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Has u-boot to be modified working with eMMC 5.1?&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;best regrads&lt;/P&gt;&lt;P&gt;René&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 29 Aug 2017 12:25:38 GMT</pubDate>
    <dc:creator>renefed</dc:creator>
    <dc:date>2017-08-29T12:25:38Z</dc:date>
    <item>
      <title>i.MX6UL u-boot doesn't recognize eMMC 5.1</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6UL-u-boot-doesn-t-recognize-eMMC-5-1/m-p/710321#M110448</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;on our custom board with i.MX6UL and eMMC 5.1, the bootloader doesn't recognize the eMMC.&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;The bootloader is loaded in serial download mode with the imx_usb_loader tool.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In uboot the following answers are shown:&lt;/P&gt;&lt;P&gt;mmc info =&amp;gt; no card present&lt;/P&gt;&lt;P&gt;mmc dev 1 =&amp;gt; Card did not respond to voltage select&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The eMMC schematic is the same as in i.MX6UL EVK.&lt;/P&gt;&lt;P&gt;The u-boot is made with fsl-arm-yocto-bsp (mx6ul_14x14_evk).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Has u-boot to be modified working with eMMC 5.1?&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;best regrads&lt;/P&gt;&lt;P&gt;René&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 29 Aug 2017 12:25:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6UL-u-boot-doesn-t-recognize-eMMC-5-1/m-p/710321#M110448</guid>
      <dc:creator>renefed</dc:creator>
      <dc:date>2017-08-29T12:25:38Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX6UL u-boot doesn't recognize eMMC 5.1</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6UL-u-boot-doesn-t-recognize-eMMC-5-1/m-p/710322#M110449</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi René&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;is emmc working in linux or freertos (for example booting from other media like sd):&lt;/P&gt;&lt;P&gt;Board Support Packages (7) &lt;BR /&gt;SDK2.2_iMX6UL_WIN(REV SDK2.2)&lt;BR /&gt;&lt;A class="jive-link-external-small" href="https://community.nxp.com/external-link.jspa?url=http%3A%2F%2Fwww.nxp.com%2Fproducts%2Fmicrocontrollers-and-processors%2Farm-processors%2Fi.mx-processors%2Fi.mx-6-processors%2Fi.mx-6ultralite-processor-low-power-secure-arm-cortex-a7-core%3Ai.MX6UL%3Ftab%3DDesign_Tools_Tab" rel="nofollow" target="_blank"&gt;http://www.nxp.com/products/microcontrollers-and-processors/arm-processors/i.mx-processors/i.mx-6-processors/i.mx-6ultralite-processor-low-power-secure-arm-cortex-a7-core:i.MX6UL?tab=Design_Tools_Tab&lt;/A&gt;&lt;/P&gt;&lt;P&gt;one can check guidelines on&lt;/P&gt;&lt;P&gt;EMMC 5.0 and EMMC 5.1 work on i.MX6 &lt;BR /&gt;&lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-332187"&gt;https://community.nxp.com/docs/DOC-332187&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 29 Aug 2017 23:28:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6UL-u-boot-doesn-t-recognize-eMMC-5-1/m-p/710322#M110449</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2017-08-29T23:28:24Z</dc:date>
    </item>
  </channel>
</rss>