<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: MIPI CSI-2 camera doesn't receive the first frame in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/MIPI-CSI-2-camera-doesn-t-receive-the-first-frame/m-p/710015#M110377</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks Igor for your confirmation.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 29 Aug 2017 11:25:51 GMT</pubDate>
    <dc:creator>titusstalin</dc:creator>
    <dc:date>2017-08-29T11:25:51Z</dc:date>
    <item>
      <title>MIPI CSI-2 camera doesn't receive the first frame</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MIPI-CSI-2-camera-doesn-t-receive-the-first-frame/m-p/710013#M110375</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Experts,&lt;/P&gt;&lt;P&gt;I have connected our MIPI CSI-2 camera to i.MX6 board.&lt;/P&gt;&lt;P&gt;And it not capturing the first frame everytime, camera sends 10 frames and i.MX receives 9frames only.&lt;/P&gt;&lt;P&gt;What could be the problem ?&lt;/P&gt;&lt;P&gt;MIPI CSI-2 i.MX host is ignoring the first frame due to avoid the unsynced frames ??&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 29 Aug 2017 07:29:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MIPI-CSI-2-camera-doesn-t-receive-the-first-frame/m-p/710013#M110375</guid>
      <dc:creator>titusstalin</dc:creator>
      <dc:date>2017-08-29T07:29:43Z</dc:date>
    </item>
    <item>
      <title>Re: MIPI CSI-2 camera doesn't receive the first frame</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MIPI-CSI-2-camera-doesn-t-receive-the-first-frame/m-p/710014#M110376</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Titus&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;you are right, if frame is started capturing in the middle,&lt;/P&gt;&lt;P&gt;it can be ignored, so capture happens after first successful frame sync&lt;/P&gt;&lt;P&gt;with second frame.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 29 Aug 2017 11:22:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MIPI-CSI-2-camera-doesn-t-receive-the-first-frame/m-p/710014#M110376</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2017-08-29T11:22:19Z</dc:date>
    </item>
    <item>
      <title>Re: MIPI CSI-2 camera doesn't receive the first frame</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MIPI-CSI-2-camera-doesn-t-receive-the-first-frame/m-p/710015#M110377</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks Igor for your confirmation.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 29 Aug 2017 11:25:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MIPI-CSI-2-camera-doesn-t-receive-the-first-frame/m-p/710015#M110377</guid>
      <dc:creator>titusstalin</dc:creator>
      <dc:date>2017-08-29T11:25:51Z</dc:date>
    </item>
  </channel>
</rss>