<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: root file system</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/root-file-system/m-p/709893#M110346</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi saida&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;please look at&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-95003"&gt;https://community.nxp.com/docs/DOC-95003&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-95046"&gt;busybox on the i.MX6 sabre sd platform in a few commands&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;also one can check&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://boundarydevices.com/trusty-ubuntu-mx6/" title="https://boundarydevices.com/trusty-ubuntu-mx6/"&gt;Trusty Ubuntu for i.MX6 boards - Boundary Devices&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;for i.MX6Q/DL differencies&lt;/P&gt;&lt;P&gt;AN4397 Common Hardware Design for i.MX 6Dual/6Quad and i.MX 6Solo/6DualLite&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://www.nxp.com/docs/en/application-note/AN4397.pdf" title="https://www.nxp.com/docs/en/application-note/AN4397.pdf"&gt;https://www.nxp.com/docs/en/application-note/AN4397.pdf&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 21 Sep 2017 23:12:19 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2017-09-21T23:12:19Z</dc:date>
    <item>
      <title>root file system</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/root-file-system/m-p/709892#M110345</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;hi&lt;/P&gt;&lt;P&gt;i am doing porting linux to sabresd board (booting from sd card)&lt;/P&gt;&lt;P&gt;1.u-boot (ok)&lt;/P&gt;&lt;P&gt;2.kernel and dtb (ok)&lt;/P&gt;&lt;P&gt;3.rootfile(ramdisk) system based on busy box (not ok)&lt;/P&gt;&lt;P&gt;i followed this from i.mx6 community "busy box on i.mx6 in few commands"&lt;/P&gt;&lt;P&gt;1. can any one give the detail procedure&lt;/P&gt;&lt;P&gt;for rootfs based on initramfs,jffs2 because i want to test it from all flash memories on board (spi flash,eMMC,sd card and nor flash)&lt;/P&gt;&lt;P&gt;2. i want to use console as a display for kernel how to do it&lt;/P&gt;&lt;P&gt;3. is it possible to port ubuntu on this board as it operates like normal pc linux os(what is the procedure for that)&lt;/P&gt;&lt;P&gt;all this i am doing seperately downloading all file from net(with out yocto)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;i am added nor flash in my custom board then what are the changes needed in u-boot and linux config files&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;4. i am designing one more board based on i.mx6 Quad core replacing with i.mx6 dual lite board what are precuations to be taken care?&lt;/P&gt;&lt;P&gt;thanks and regards&lt;/P&gt;&lt;P&gt;saida&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 21 Sep 2017 06:06:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/root-file-system/m-p/709892#M110345</guid>
      <dc:creator>saida</dc:creator>
      <dc:date>2017-09-21T06:06:24Z</dc:date>
    </item>
    <item>
      <title>Re: root file system</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/root-file-system/m-p/709893#M110346</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi saida&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;please look at&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-95003"&gt;https://community.nxp.com/docs/DOC-95003&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-95046"&gt;busybox on the i.MX6 sabre sd platform in a few commands&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;also one can check&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://boundarydevices.com/trusty-ubuntu-mx6/" title="https://boundarydevices.com/trusty-ubuntu-mx6/"&gt;Trusty Ubuntu for i.MX6 boards - Boundary Devices&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;for i.MX6Q/DL differencies&lt;/P&gt;&lt;P&gt;AN4397 Common Hardware Design for i.MX 6Dual/6Quad and i.MX 6Solo/6DualLite&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://www.nxp.com/docs/en/application-note/AN4397.pdf" title="https://www.nxp.com/docs/en/application-note/AN4397.pdf"&gt;https://www.nxp.com/docs/en/application-note/AN4397.pdf&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 21 Sep 2017 23:12:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/root-file-system/m-p/709893#M110346</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2017-09-21T23:12:19Z</dc:date>
    </item>
    <item>
      <title>Re: root file system</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/root-file-system/m-p/709894#M110347</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;hi igorpadykov&lt;/P&gt;&lt;P&gt;i will try and come back to you&lt;/P&gt;&lt;P&gt;thank you&lt;/P&gt;&lt;P&gt;regards saida&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 25 Sep 2017 16:58:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/root-file-system/m-p/709894#M110347</guid>
      <dc:creator>saida</dc:creator>
      <dc:date>2017-09-25T16:58:38Z</dc:date>
    </item>
    <item>
      <title>Re: root file system</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/root-file-system/m-p/709895#M110348</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;hi igorpadykov&lt;/P&gt;&lt;P&gt;its working&lt;/P&gt;&lt;P&gt;but i want to make it standalone using parallel nor flash memory&lt;/P&gt;&lt;P&gt;my custom board is based on sabresd board and i added parallel nor flash on EIM bus (8MB)&lt;/P&gt;&lt;P&gt;i can flash do u-boot.imx and kernel image on nor flash but i want to mount rootfs on it&lt;/P&gt;&lt;P&gt;how i can do this can you send any docs regarding this ?&lt;/P&gt;&lt;P&gt;thank you&lt;/P&gt;&lt;P&gt;regards&lt;/P&gt;&lt;P&gt;Saida&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 27 Sep 2017 17:55:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/root-file-system/m-p/709895#M110348</guid>
      <dc:creator>saida</dc:creator>
      <dc:date>2017-09-27T17:55:06Z</dc:date>
    </item>
  </channel>
</rss>