<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Sound Solution implementation for IMx6 using PCM1754-Q1 DAC with ESAI Interface</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Sound-Solution-implementation-for-IMx6-using-PCM1754-Q1-DAC-with/m-p/709222#M110251</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi All&lt;/P&gt;&lt;P&gt;Need to design a sound solution with IMx6 ESAI Interface using PCM1754-Q1 DAC&lt;/P&gt;&lt;P&gt;44.1 KHz sample rate audio input (16bit PCM Data) and single channel (right channel) output&lt;/P&gt;&lt;P&gt;Data Format configured in PCM1754-Q1 is 16bit I2S Format&lt;/P&gt;&lt;P&gt;Anybody has tried the solution for the above mentioned specs earlier ?&lt;/P&gt;&lt;P&gt;If not, what will be the ESAI Clock settings (SCK, BCK and LRCK)&amp;nbsp; for the above mentioned specs ?&lt;/P&gt;&lt;P&gt;ESAI Clock source should be PLL4 and 22.5792MHz System clock frequency is needed as per PCM1754-Q1 Datasheet&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 29 Aug 2017 10:30:06 GMT</pubDate>
    <dc:creator>vigneshm93</dc:creator>
    <dc:date>2017-08-29T10:30:06Z</dc:date>
    <item>
      <title>Sound Solution implementation for IMx6 using PCM1754-Q1 DAC with ESAI Interface</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Sound-Solution-implementation-for-IMx6-using-PCM1754-Q1-DAC-with/m-p/709222#M110251</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi All&lt;/P&gt;&lt;P&gt;Need to design a sound solution with IMx6 ESAI Interface using PCM1754-Q1 DAC&lt;/P&gt;&lt;P&gt;44.1 KHz sample rate audio input (16bit PCM Data) and single channel (right channel) output&lt;/P&gt;&lt;P&gt;Data Format configured in PCM1754-Q1 is 16bit I2S Format&lt;/P&gt;&lt;P&gt;Anybody has tried the solution for the above mentioned specs earlier ?&lt;/P&gt;&lt;P&gt;If not, what will be the ESAI Clock settings (SCK, BCK and LRCK)&amp;nbsp; for the above mentioned specs ?&lt;/P&gt;&lt;P&gt;ESAI Clock source should be PLL4 and 22.5792MHz System clock frequency is needed as per PCM1754-Q1 Datasheet&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 29 Aug 2017 10:30:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Sound-Solution-implementation-for-IMx6-using-PCM1754-Q1-DAC-with/m-p/709222#M110251</guid>
      <dc:creator>vigneshm93</dc:creator>
      <dc:date>2017-08-29T10:30:06Z</dc:date>
    </item>
    <item>
      <title>Re: Sound Solution implementation for IMx6 using PCM1754-Q1 DAC with ESAI Interface</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Sound-Solution-implementation-for-IMx6-using-PCM1754-Q1-DAC-with/m-p/709223#M110252</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Vignesh&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;esai is supported on i.MX6Q Sabre AI board:&lt;/P&gt;&lt;P&gt;Schematics (5)&lt;BR /&gt;Design files for i.MX 6Quad and i.MX 6DualLite CPU1 Cards &lt;BR /&gt;Design files for Base Board&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.nxp.com/products/software-and-tools/hardware-development-tools/sabre-development-system/sabre-for-automotive-infotainment-based-on-the-i.mx-6-series:RDIMX6SABREAUTO?fpsp=1&amp;amp;tab=Design_Tools_Tab"&gt;http://www.nxp.com/products/software-and-tools/hardware-development-tools/sabre-development-system/sabre-for-automotive-infotainment-based-on-the-i.mx-6-series:RDIMX6SABREAUTO?fpsp=1&amp;amp;tab=Design_Tools_Tab&lt;/A&gt;&lt;/P&gt;&lt;P&gt;Linux driver description is provided in Chapter 28 Advanced Linux Sound Architecture (ALSA) System on a Chip (ASoC)&lt;/P&gt;&lt;P&gt;Sound Driver attached Linux Manual.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 29 Aug 2017 23:33:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Sound-Solution-implementation-for-IMx6-using-PCM1754-Q1-DAC-with/m-p/709223#M110252</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2017-08-29T23:33:23Z</dc:date>
    </item>
  </channel>
</rss>