<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: IMX6Q usb HOST in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/IMX6Q-usb-HOST/m-p/709170#M110239</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Q[translated by Google]:&lt;/P&gt;&lt;P&gt;imx6q can not identify U disk, then usb mouse can be identified:&lt;BR /&gt;PCB must do 90 ohm impedance? What is the reason for this?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;A:&lt;/P&gt;&lt;P&gt;Hi &amp;nbsp;小辉哥&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;yes reason may be poor signal, note mouse is detected as low speed device.&lt;/P&gt;&lt;P&gt;One can look at AN4589 Configuring USB on i.MX6 Series Processors&amp;nbsp;&lt;/P&gt;&lt;P&gt;sect.4.3.3 Operational settings for settings to tweak signal&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://cache.nxp.com/docs/en/application-note/AN4589.pdf" title="https://cache.nxp.com/docs/en/application-note/AN4589.pdf"&gt;https://cache.nxp.com/docs/en/application-note/AN4589.pdf&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 20 Sep 2017 23:16:14 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2017-09-20T23:16:14Z</dc:date>
    <item>
      <title>IMX6Q usb HOST</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6Q-usb-HOST/m-p/709169#M110238</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;imx6q 识别不了U盘，接上usb鼠标可以识别到：&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_2.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/31420i1A7FD1285DA1EFCF/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_2.png" alt="pastedImage_2.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;PCB一定要做90欧的阻抗吗？这个大概是什么原因导致的呢？&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 20 Sep 2017 09:04:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6Q-usb-HOST/m-p/709169#M110238</guid>
      <dc:creator>小辉哥</dc:creator>
      <dc:date>2017-09-20T09:04:23Z</dc:date>
    </item>
    <item>
      <title>Re: IMX6Q usb HOST</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6Q-usb-HOST/m-p/709170#M110239</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Q[translated by Google]:&lt;/P&gt;&lt;P&gt;imx6q can not identify U disk, then usb mouse can be identified:&lt;BR /&gt;PCB must do 90 ohm impedance? What is the reason for this?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;A:&lt;/P&gt;&lt;P&gt;Hi &amp;nbsp;小辉哥&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;yes reason may be poor signal, note mouse is detected as low speed device.&lt;/P&gt;&lt;P&gt;One can look at AN4589 Configuring USB on i.MX6 Series Processors&amp;nbsp;&lt;/P&gt;&lt;P&gt;sect.4.3.3 Operational settings for settings to tweak signal&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://cache.nxp.com/docs/en/application-note/AN4589.pdf" title="https://cache.nxp.com/docs/en/application-note/AN4589.pdf"&gt;https://cache.nxp.com/docs/en/application-note/AN4589.pdf&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 20 Sep 2017 23:16:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6Q-usb-HOST/m-p/709170#M110239</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2017-09-20T23:16:14Z</dc:date>
    </item>
  </channel>
</rss>