<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックCapture only 1 field on BT656 interlaced input</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Capture-only-1-field-on-BT656-interlaced-input/m-p/708621#M110109</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Is it possible to have the mxc overlay feature only capture the 1st field of an interlaced BT656 input? &amp;nbsp;We can do this on an interlaced MIPI input by setting the input window (CSIx ACT FRAME SIZE REGISTER) height to the height of 1 field. &amp;nbsp;We tried similarly for BT656 but it just doesnt seem to work. &amp;nbsp;We use the iMX6 solo and&amp;nbsp;dual processors.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 28 Aug 2017 02:02:27 GMT</pubDate>
    <dc:creator>richogrady</dc:creator>
    <dc:date>2017-08-28T02:02:27Z</dc:date>
    <item>
      <title>Capture only 1 field on BT656 interlaced input</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Capture-only-1-field-on-BT656-interlaced-input/m-p/708621#M110109</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Is it possible to have the mxc overlay feature only capture the 1st field of an interlaced BT656 input? &amp;nbsp;We can do this on an interlaced MIPI input by setting the input window (CSIx ACT FRAME SIZE REGISTER) height to the height of 1 field. &amp;nbsp;We tried similarly for BT656 but it just doesnt seem to work. &amp;nbsp;We use the iMX6 solo and&amp;nbsp;dual processors.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 28 Aug 2017 02:02:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Capture-only-1-field-on-BT656-interlaced-input/m-p/708621#M110109</guid>
      <dc:creator>richogrady</dc:creator>
      <dc:date>2017-08-28T02:02:27Z</dc:date>
    </item>
    <item>
      <title>Re: Capture only 1 field on BT656 interlaced input</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Capture-only-1-field-on-BT656-interlaced-input/m-p/708622#M110110</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&amp;nbsp;We can do this on an interlaced MIPI input by setting the input window&lt;/P&gt;&lt;P&gt;&amp;gt; what mipi input format do you use if not bt656?&lt;/P&gt;&lt;P&gt;maybe you can capture by your own software, since they stored in the memory field by field.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 28 Aug 2017 09:31:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Capture-only-1-field-on-BT656-interlaced-input/m-p/708622#M110110</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2017-08-28T09:31:57Z</dc:date>
    </item>
    <item>
      <title>Re: Capture only 1 field on BT656 interlaced input</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Capture-only-1-field-on-BT656-interlaced-input/m-p/708623#M110111</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;To clarify: the MIPI input is BT656 in contrast to the parallel BT656 input. &amp;nbsp;The goal is to capture as non-interlaced so the fields sit in memory one after another (i.e. are not deinterlaced), and then crop to the one field. &amp;nbsp;Form here the image can be scaled on output. &amp;nbsp;Works just fine on the MIPI BT656 input, why can't it work on the parallel BT656 input?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 28 Aug 2017 13:42:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Capture-only-1-field-on-BT656-interlaced-input/m-p/708623#M110111</guid>
      <dc:creator>richogrady</dc:creator>
      <dc:date>2017-08-28T13:42:21Z</dc:date>
    </item>
  </channel>
</rss>