<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Digital IO voltages PF3000 in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Digital-IO-voltages-PF3000/m-p/708218#M110038</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;In the datasheet of the PF3000 is the Vol max = 0.4*Vddio. When Vddio = 3.3V the Vol max is 1.32V and this is really high. in comparison to PF2000 is the Vol max 0.4V. is the 0.4V*Vddio correct because i will use the&amp;nbsp;i.MX6SX connected to the PF3000?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 17 Oct 2017 09:27:39 GMT</pubDate>
    <dc:creator>maartengeurts</dc:creator>
    <dc:date>2017-10-17T09:27:39Z</dc:date>
    <item>
      <title>Digital IO voltages PF3000</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Digital-IO-voltages-PF3000/m-p/708218#M110038</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;In the datasheet of the PF3000 is the Vol max = 0.4*Vddio. When Vddio = 3.3V the Vol max is 1.32V and this is really high. in comparison to PF2000 is the Vol max 0.4V. is the 0.4V*Vddio correct because i will use the&amp;nbsp;i.MX6SX connected to the PF3000?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 17 Oct 2017 09:27:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Digital-IO-voltages-PF3000/m-p/708218#M110038</guid>
      <dc:creator>maartengeurts</dc:creator>
      <dc:date>2017-10-17T09:27:39Z</dc:date>
    </item>
    <item>
      <title>Re: Digital IO voltages PF3000</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Digital-IO-voltages-PF3000/m-p/708219#M110039</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;gt;&amp;gt;is the 0.4V*Vddio correct because i will use the&amp;nbsp;i.MX6SX connected to the PF3000?&lt;/P&gt;&lt;P&gt;Yes, it is. Don't worry about it. It doesn't affect your application.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;TIC&amp;nbsp;&amp;nbsp; Weidong&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 11 Jan 2018 06:24:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Digital-IO-voltages-PF3000/m-p/708219#M110039</guid>
      <dc:creator>weidong_sun</dc:creator>
      <dc:date>2018-01-11T06:24:08Z</dc:date>
    </item>
  </channel>
</rss>