<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic USB2 host in u-boot in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/USB2-host-in-u-boot/m-p/707564#M109957</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;We are trying to find our modem that is connected to USB2 on our custom imx6ull board. The USB block gets power since we are booting from MFGtool to get into u-boot. But the modem can not be found when running the usb start command. The board is based around the EVK and out u-boot is based around the EVK config.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Does the second USB port needs to be configured from default to support host mode?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 25 Aug 2017 20:15:08 GMT</pubDate>
    <dc:creator>pyraohms</dc:creator>
    <dc:date>2017-08-25T20:15:08Z</dc:date>
    <item>
      <title>USB2 host in u-boot</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/USB2-host-in-u-boot/m-p/707564#M109957</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;We are trying to find our modem that is connected to USB2 on our custom imx6ull board. The USB block gets power since we are booting from MFGtool to get into u-boot. But the modem can not be found when running the usb start command. The board is based around the EVK and out u-boot is based around the EVK config.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Does the second USB port needs to be configured from default to support host mode?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 25 Aug 2017 20:15:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/USB2-host-in-u-boot/m-p/707564#M109957</guid>
      <dc:creator>pyraohms</dc:creator>
      <dc:date>2017-08-25T20:15:08Z</dc:date>
    </item>
    <item>
      <title>Re: USB2 host in u-boot</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/USB2-host-in-u-boot/m-p/707565#M109958</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Per&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;one can check if signal usb_id is low. Is modem working fine with usb1.&lt;/P&gt;&lt;P&gt;Also modems may consume much current, one can try to test with usb stick.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 25 Aug 2017 23:02:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/USB2-host-in-u-boot/m-p/707565#M109958</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2017-08-25T23:02:46Z</dc:date>
    </item>
  </channel>
</rss>