<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic i.mx6q hangs at Starting kernel log daemon... in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-mx6q-hangs-at-Starting-kernel-log-daemon/m-p/707399#M109936</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The hardware is i.mx6q sabresd board.&amp;nbsp;&lt;/P&gt;&lt;P&gt;The rootfs I'm using is&amp;nbsp;fsl-image-qt5-validation-imx-fb-imx6qdlsolo in L4.1.15_2.0.0-ga_images_MX6QDLSOLO, and I don't modify the rootfs.&lt;/P&gt;&lt;P&gt;The Linux version is&amp;nbsp;imx_4.1.15_2.0.0_ga.&lt;/P&gt;&lt;P&gt;The rootfs is mounted through NFS.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When I boot the board, it hangs on&amp;nbsp;Starting kernel log daemon... for a long time (about several minutes), and then it hands at&amp;nbsp;umount: /mnt/.psplash: umount failed: No such file or directory. The print log is:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;.........&lt;/P&gt;&lt;P&gt;/etc/network/if-pre-up.d/nfsroot: line 12: /proc/mounts: No such file or directory&lt;BR /&gt;run-parts: /etc/network/if-pre-up.d/nfsroot: exit status 1&lt;BR /&gt;Starting system message bus: Failed to start message bus: Failed to bind socket "/var/run/dbus/system_bus_socket": No such file or directory&lt;BR /&gt;dbus.&lt;BR /&gt;/etc/rc5.d/S05connman: line 15: /proc/mounts: No such file or directory&lt;BR /&gt;/etc/rc5.d/S10dropbear: line 32: /proc/mounts: No such file or directory&lt;BR /&gt;Starting Dropbear SSH server: dropbear.&lt;BR /&gt;Starting rpcbind daemon...done.&lt;BR /&gt;starting statd: done&lt;BR /&gt;Starting advanced power management daemon: No APM support in kernel&lt;BR /&gt;(failed.)&lt;BR /&gt;Starting atd: OK&lt;BR /&gt;exportfs: can't open /etc/exports for reading&lt;BR /&gt;grep: /proc/filesystems: No such file or directory&lt;BR /&gt;NFS daemon support not enabled in kernel&lt;BR /&gt;Starting system log daemon...0&lt;BR /&gt;&lt;STRONG&gt;Starting kernel log daemon...&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt; * Starting Avahi mDNS/DNS-SD Daemon: avahi-daemon [fail]&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;Starting Telephony daemon&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;Starting Linux NFC daemon&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;Failed to connect to socket /var/run/dbus/system_bus_socket: No such file or directory&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;Starting crond: OK&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;Running local boot scripts (/etc/rc.local)/etc/rc.local: line 15: /proc/sys/vm/min_free_kbytes: No such file or directory&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;error&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;umount: /mnt/.psplash: umount failed: No such file or directory&lt;/STRONG&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 25 Aug 2017 02:36:58 GMT</pubDate>
    <dc:creator>shijunzhao</dc:creator>
    <dc:date>2017-08-25T02:36:58Z</dc:date>
    <item>
      <title>i.mx6q hangs at Starting kernel log daemon...</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-mx6q-hangs-at-Starting-kernel-log-daemon/m-p/707399#M109936</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The hardware is i.mx6q sabresd board.&amp;nbsp;&lt;/P&gt;&lt;P&gt;The rootfs I'm using is&amp;nbsp;fsl-image-qt5-validation-imx-fb-imx6qdlsolo in L4.1.15_2.0.0-ga_images_MX6QDLSOLO, and I don't modify the rootfs.&lt;/P&gt;&lt;P&gt;The Linux version is&amp;nbsp;imx_4.1.15_2.0.0_ga.&lt;/P&gt;&lt;P&gt;The rootfs is mounted through NFS.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When I boot the board, it hangs on&amp;nbsp;Starting kernel log daemon... for a long time (about several minutes), and then it hands at&amp;nbsp;umount: /mnt/.psplash: umount failed: No such file or directory. The print log is:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;.........&lt;/P&gt;&lt;P&gt;/etc/network/if-pre-up.d/nfsroot: line 12: /proc/mounts: No such file or directory&lt;BR /&gt;run-parts: /etc/network/if-pre-up.d/nfsroot: exit status 1&lt;BR /&gt;Starting system message bus: Failed to start message bus: Failed to bind socket "/var/run/dbus/system_bus_socket": No such file or directory&lt;BR /&gt;dbus.&lt;BR /&gt;/etc/rc5.d/S05connman: line 15: /proc/mounts: No such file or directory&lt;BR /&gt;/etc/rc5.d/S10dropbear: line 32: /proc/mounts: No such file or directory&lt;BR /&gt;Starting Dropbear SSH server: dropbear.&lt;BR /&gt;Starting rpcbind daemon...done.&lt;BR /&gt;starting statd: done&lt;BR /&gt;Starting advanced power management daemon: No APM support in kernel&lt;BR /&gt;(failed.)&lt;BR /&gt;Starting atd: OK&lt;BR /&gt;exportfs: can't open /etc/exports for reading&lt;BR /&gt;grep: /proc/filesystems: No such file or directory&lt;BR /&gt;NFS daemon support not enabled in kernel&lt;BR /&gt;Starting system log daemon...0&lt;BR /&gt;&lt;STRONG&gt;Starting kernel log daemon...&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt; * Starting Avahi mDNS/DNS-SD Daemon: avahi-daemon [fail]&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;Starting Telephony daemon&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;Starting Linux NFC daemon&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;Failed to connect to socket /var/run/dbus/system_bus_socket: No such file or directory&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;Starting crond: OK&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;Running local boot scripts (/etc/rc.local)/etc/rc.local: line 15: /proc/sys/vm/min_free_kbytes: No such file or directory&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;error&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;umount: /mnt/.psplash: umount failed: No such file or directory&lt;/STRONG&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 25 Aug 2017 02:36:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-mx6q-hangs-at-Starting-kernel-log-daemon/m-p/707399#M109936</guid>
      <dc:creator>shijunzhao</dc:creator>
      <dc:date>2017-08-25T02:36:58Z</dc:date>
    </item>
    <item>
      <title>Re: i.mx6q hangs at Starting kernel log daemon...</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-mx6q-hangs-at-Starting-kernel-log-daemon/m-p/707400#M109937</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;try to use the command :&lt;/P&gt;&lt;P&gt;sudo chmod 777 -R &amp;lt;your Yocto work folder&amp;gt;/fsl-image-qt5/1.0-r0/rootfs, then try build again.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 29 Aug 2017 08:25:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-mx6q-hangs-at-Starting-kernel-log-daemon/m-p/707400#M109937</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2017-08-29T08:25:53Z</dc:date>
    </item>
    <item>
      <title>Re: i.mx6q hangs at Starting kernel log daemon...</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-mx6q-hangs-at-Starting-kernel-log-daemon/m-p/707401#M109938</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I don't find your path. I'm using following build commands:&lt;/P&gt;&lt;P style="background: white;"&gt;&lt;SPAN style="font-size: 12.0pt; color: black;"&gt;$MACHINE=imx6qsabresd DISTRO=fsl-imx-x11 source ./fsl-setup-release.sh -b bld-x11&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="background: white;"&gt;&lt;SPAN style="font-size: 12.0pt; color: black;"&gt;$bitbake&amp;nbsp;fsl-image-gui&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 31 Aug 2017 07:19:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-mx6q-hangs-at-Starting-kernel-log-daemon/m-p/707401#M109938</guid>
      <dc:creator>shijunzhao</dc:creator>
      <dc:date>2017-08-31T07:19:59Z</dc:date>
    </item>
    <item>
      <title>Re: i.mx6q hangs at Starting kernel log daemon...</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-mx6q-hangs-at-Starting-kernel-log-daemon/m-p/707402#M109939</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;if you use x11 image, you can find your "work" folder under build_x11/tmp/work, can you find it? then find the "rootfs" folder under work/imx6xxx(board name)/fsl-image-gui/1.0-r.0/rootfs&lt;/P&gt;&lt;P&gt;if you can find this folder, try to use the command as I mentioned last time, change the path to your own path. then build again.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 31 Aug 2017 08:45:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-mx6q-hangs-at-Starting-kernel-log-daemon/m-p/707402#M109939</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2017-08-31T08:45:42Z</dc:date>
    </item>
  </channel>
</rss>