<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: bitbake debug mode (-DDD) no errors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/bitbake-debug-mode-DDD-no-errors/m-p/706752#M109830</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;you can read the log file in imx-test/1_5.7-r0/temp/log.do_compile&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 21 Sep 2017 08:38:03 GMT</pubDate>
    <dc:creator>jimmychan</dc:creator>
    <dc:date>2017-09-21T08:38:03Z</dc:date>
    <item>
      <title>bitbake debug mode (-DDD) no errors</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/bitbake-debug-mode-DDD-no-errors/m-p/706751#M109829</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have setup the yocto build system on my pc.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm working on i.MX 7 Dual SABRE board.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;First I did&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;bitbake imx-test&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Which fetched and built the latest imx-test package in my build directory.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What I wanted to do was,&lt;/P&gt;&lt;P&gt;make changes in the source code of the programs in imx-test package and compile them using bitbake.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So I made my changes and tried&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;bitbake -c compile -f imx-test&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Which compiled the imx-test package with modified source code.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But the output binary files did not generate, because my code had some errors in it.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So I tried&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;bitbake -c compile -f imx-test -DDD&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Which gave a lot of debug information, but none about the errors in my code.&lt;/P&gt;&lt;P&gt;The surprising thing was that the compile task was shown to be successful, even with the errors in my code.&lt;/P&gt;&lt;P&gt;But the output binaries were not generated because of the errors.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What is the highest level of debug mode in bitbake?&lt;/P&gt;&lt;P&gt;Is there any way to view the errors in my code using bitbake?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please help asap.&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 18 Sep 2017 18:32:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/bitbake-debug-mode-DDD-no-errors/m-p/706751#M109829</guid>
      <dc:creator>arsadhusainmomi</dc:creator>
      <dc:date>2017-09-18T18:32:34Z</dc:date>
    </item>
    <item>
      <title>Re: bitbake debug mode (-DDD) no errors</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/bitbake-debug-mode-DDD-no-errors/m-p/706752#M109830</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;you can read the log file in imx-test/1_5.7-r0/temp/log.do_compile&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 21 Sep 2017 08:38:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/bitbake-debug-mode-DDD-no-errors/m-p/706752#M109830</guid>
      <dc:creator>jimmychan</dc:creator>
      <dc:date>2017-09-21T08:38:03Z</dc:date>
    </item>
  </channel>
</rss>