<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Recompiling MFGTool</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Recompiling-MFGTool/m-p/706443#M109784</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We have custom iMX6Q based HW. I remember last time it being really pain to get MFGTool recompiled but somehow I managed.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Now there was modification to HW and I need to update MFGTool Linux system as well. I managed to get it compiled and it boots but always stops at this:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;ALSA device list:&lt;BR /&gt; No soundcards found.&lt;BR /&gt;Freeing unused kernel memory: 736K (80cee000 - 80da6000)&lt;BR /&gt;Starting UTP&lt;BR /&gt;uuc 0.5 [built Aug 24 2017 06:21:04]&lt;BR /&gt;UTP: Waiting for device to appear&lt;/P&gt;&lt;P&gt;UTP: file/device node /dev/utp already exist&lt;/P&gt;&lt;P&gt;cpu_id is 0&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;Nothing happens after that.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm using Yocto 2.2 (morty) and latest meta-freescale - layer version. Linux kernel version is 4.1.15&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I made sure that I was using the imx_v7_mfg_defconfig stated in the manual but that didn't help any.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Has anyone managed to recompile mfgtools with Yocto 2.1 or 2.2 or any idea what might be the problem?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This is the same problem I was having with the older 3.10.17 kernel based Yocto, but there I got it sorted someway. I just don't remember anymore how.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 24 Aug 2017 09:22:08 GMT</pubDate>
    <dc:creator>Maddis</dc:creator>
    <dc:date>2017-08-24T09:22:08Z</dc:date>
    <item>
      <title>Recompiling MFGTool</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Recompiling-MFGTool/m-p/706443#M109784</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We have custom iMX6Q based HW. I remember last time it being really pain to get MFGTool recompiled but somehow I managed.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Now there was modification to HW and I need to update MFGTool Linux system as well. I managed to get it compiled and it boots but always stops at this:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;ALSA device list:&lt;BR /&gt; No soundcards found.&lt;BR /&gt;Freeing unused kernel memory: 736K (80cee000 - 80da6000)&lt;BR /&gt;Starting UTP&lt;BR /&gt;uuc 0.5 [built Aug 24 2017 06:21:04]&lt;BR /&gt;UTP: Waiting for device to appear&lt;/P&gt;&lt;P&gt;UTP: file/device node /dev/utp already exist&lt;/P&gt;&lt;P&gt;cpu_id is 0&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;Nothing happens after that.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm using Yocto 2.2 (morty) and latest meta-freescale - layer version. Linux kernel version is 4.1.15&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I made sure that I was using the imx_v7_mfg_defconfig stated in the manual but that didn't help any.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Has anyone managed to recompile mfgtools with Yocto 2.1 or 2.2 or any idea what might be the problem?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This is the same problem I was having with the older 3.10.17 kernel based Yocto, but there I got it sorted someway. I just don't remember anymore how.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 24 Aug 2017 09:22:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Recompiling-MFGTool/m-p/706443#M109784</guid>
      <dc:creator>Maddis</dc:creator>
      <dc:date>2017-08-24T09:22:08Z</dc:date>
    </item>
    <item>
      <title>Re: Recompiling MFGTool</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Recompiling-MFGTool/m-p/706444#M109785</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi mc&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;this may be caused by low usb_id pin as on&lt;/P&gt;&lt;P&gt;&lt;A class="jive-link-thread-small" data-containerid="2004" data-containertype="14" data-objectid="365690" data-objecttype="1" href="https://community.nxp.com/thread/365690"&gt;https://community.nxp.com/thread/365690&lt;/A&gt;&lt;BR /&gt;&lt;A _jive_internal="true" href="https://community.nxp.com/thread/375912"&gt;https://community.nxp.com/thread/375912&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 24 Aug 2017 23:08:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Recompiling-MFGTool/m-p/706444#M109785</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2017-08-24T23:08:02Z</dc:date>
    </item>
    <item>
      <title>Re: Recompiling MFGTool</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Recompiling-MFGTool/m-p/706445#M109786</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;This was in fact the case! I went through the device tree and fixed the pin and now the mfgtool system boots and update starts!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 25 Aug 2017 05:03:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Recompiling-MFGTool/m-p/706445#M109786</guid>
      <dc:creator>Maddis</dc:creator>
      <dc:date>2017-08-25T05:03:13Z</dc:date>
    </item>
  </channel>
</rss>