<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックHDMI - Resolution Isuue</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/HDMI-Resolution-Isuue/m-p/706217#M109744</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am working on imx6Q board with linux yocto 3.14.38.&lt;/P&gt;&lt;P&gt;Please clarify the following observations.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1.In Uboot, I have set &lt;A href="mailto:1920x1080@60"&gt;1920x1080@60&lt;/A&gt;&amp;nbsp;and connected the 1920x1080 hdmi monitor, then the image looks proper and fbset shows the proper values for resolution as 1920x1080.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If i connect other lower resolution monitor (1280x720) ,The image looks like 640x480 and when verified with fbset, it shows 640x480&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;2.If the resolution is changed to &lt;A href="mailto:1280x720@60"&gt;1280x720@60&lt;/A&gt;&amp;nbsp;during uboot, The image looks proper on 1280x720 Monitor.&lt;/P&gt;&lt;P&gt;If the same is connected to 1920x1080 monitor.It shows big icons and fbset shows the resolution as &lt;A href="mailto:640x480@60"&gt;640x480@60&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;How does the resolution differs on HDMI monitor.Is it due to HDMI monitor settings or due to settings in Linux BSP.&lt;/P&gt;&lt;P&gt;Please clarify&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks and Regards&lt;/P&gt;&lt;P&gt;Rizwan Syed&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 18 Sep 2017 13:20:44 GMT</pubDate>
    <dc:creator>rizwan_s</dc:creator>
    <dc:date>2017-09-18T13:20:44Z</dc:date>
    <item>
      <title>HDMI - Resolution Isuue</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/HDMI-Resolution-Isuue/m-p/706217#M109744</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am working on imx6Q board with linux yocto 3.14.38.&lt;/P&gt;&lt;P&gt;Please clarify the following observations.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1.In Uboot, I have set &lt;A href="mailto:1920x1080@60"&gt;1920x1080@60&lt;/A&gt;&amp;nbsp;and connected the 1920x1080 hdmi monitor, then the image looks proper and fbset shows the proper values for resolution as 1920x1080.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If i connect other lower resolution monitor (1280x720) ,The image looks like 640x480 and when verified with fbset, it shows 640x480&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;2.If the resolution is changed to &lt;A href="mailto:1280x720@60"&gt;1280x720@60&lt;/A&gt;&amp;nbsp;during uboot, The image looks proper on 1280x720 Monitor.&lt;/P&gt;&lt;P&gt;If the same is connected to 1920x1080 monitor.It shows big icons and fbset shows the resolution as &lt;A href="mailto:640x480@60"&gt;640x480@60&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;How does the resolution differs on HDMI monitor.Is it due to HDMI monitor settings or due to settings in Linux BSP.&lt;/P&gt;&lt;P&gt;Please clarify&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks and Regards&lt;/P&gt;&lt;P&gt;Rizwan Syed&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 18 Sep 2017 13:20:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/HDMI-Resolution-Isuue/m-p/706217#M109744</guid>
      <dc:creator>rizwan_s</dc:creator>
      <dc:date>2017-09-18T13:20:44Z</dc:date>
    </item>
    <item>
      <title>Re: HDMI - Resolution Isuue</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/HDMI-Resolution-Isuue/m-p/706218#M109745</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Rizwan&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;please look at splashscreen patches on&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-98109"&gt;Patch to support uboot logo keep from uboot to kernel for NXP Linux and Android BSP (HDMI, LCD and LVDS)&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;seems 640x480 is default resolution so it is used if any problem happens.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 18 Sep 2017 23:40:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/HDMI-Resolution-Isuue/m-p/706218#M109745</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2017-09-18T23:40:28Z</dc:date>
    </item>
  </channel>
</rss>