<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Is the i.MX6ULL drop-in compatible with the i.MX6UL?</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Is-the-i-MX6ULL-drop-in-compatible-with-the-i-MX6UL/m-p/706107#M109708</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&amp;nbsp;Basically i.MX6ULL is pin-to-pin compatible with i.MX6UL. Your may look &lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;at i.MX 6ULL Migration Guide for more details about i.MX6ULL and i.MX6UL&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;differences. &lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&amp;nbsp;As for 1.375V (1.4V) for DDR3L device - it makes sense to consult with DRAM &lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;manufacturer. &lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&amp;nbsp; Correct, i.MX6ULL does not have ERR009455 (Clock: 24 MHz Oscillator does &lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;not start up), that was detected for i.MX6UL of revision 1.0.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://www.nxp.com/docs/en/application-note/AN5350.pdf" title="https://www.nxp.com/docs/en/application-note/AN5350.pdf"&gt;https://www.nxp.com/docs/en/application-note/AN5350.pdf&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Yuri&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 16 Oct 2017 08:12:32 GMT</pubDate>
    <dc:creator>Yuri</dc:creator>
    <dc:date>2017-10-16T08:12:32Z</dc:date>
    <item>
      <title>Is the i.MX6ULL drop-in compatible with the i.MX6UL?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Is-the-i-MX6ULL-drop-in-compatible-with-the-i-MX6UL/m-p/706106#M109707</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I looked through the datasheet of the i.MX6ULL, and at least the 14x14 package seems to have the same pinning as the i.MX6UL. Are these drop-in compatible? Oddly, I didn't see any documentation that explicitly mentioned this (strange, as this is really a nice feature to have — and the other i.MX6s brag about it :-) ).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I've been getting a custom i.MX6UL board up and running, and since I'm about to order a new revision, I'm wondering what changes I need to make if I want to switch over to the 900 MHz i.MX6ULL? I'm looking at the&amp;nbsp;MCIMX6Y2DVM09AA, which is only $1 more than the 535 MHz&amp;nbsp;MCIMX6Y0CVM05AA I'm using right now.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The big difference I see is the minimum VDD_SOC_IN voltage. Since power consumption isn't critical for my application, I'm currently using a discrete DC/DC converter to generate a 1.35V rail that's shared by VDD_SOC_IN and my DDR3L memory (I really appreciate the built-in LDOs on the i.MX6 — thanks for that!)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;However, the ULL needs a minimum of 1.375V. If I bump my regulator from 1.35 to 1.4V, that should provide enough margin, while still operating my DDR3L within bounds. Cool?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Looking at the errata, it doesn't look like the ULL has the crystal oscillator bug that the UL has. Is this correct?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Anything else I should be thinking about?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 14 Oct 2017 03:46:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Is-the-i-MX6ULL-drop-in-compatible-with-the-i-MX6UL/m-p/706106#M109707</guid>
      <dc:creator>jay_d_carlson</dc:creator>
      <dc:date>2017-10-14T03:46:02Z</dc:date>
    </item>
    <item>
      <title>Re: Is the i.MX6ULL drop-in compatible with the i.MX6UL?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Is-the-i-MX6ULL-drop-in-compatible-with-the-i-MX6UL/m-p/706107#M109708</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&amp;nbsp;Basically i.MX6ULL is pin-to-pin compatible with i.MX6UL. Your may look &lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;at i.MX 6ULL Migration Guide for more details about i.MX6ULL and i.MX6UL&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;differences. &lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&amp;nbsp;As for 1.375V (1.4V) for DDR3L device - it makes sense to consult with DRAM &lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;manufacturer. &lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&amp;nbsp; Correct, i.MX6ULL does not have ERR009455 (Clock: 24 MHz Oscillator does &lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;not start up), that was detected for i.MX6UL of revision 1.0.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://www.nxp.com/docs/en/application-note/AN5350.pdf" title="https://www.nxp.com/docs/en/application-note/AN5350.pdf"&gt;https://www.nxp.com/docs/en/application-note/AN5350.pdf&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Yuri&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 16 Oct 2017 08:12:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Is-the-i-MX6ULL-drop-in-compatible-with-the-i-MX6UL/m-p/706107#M109708</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2017-10-16T08:12:32Z</dc:date>
    </item>
    <item>
      <title>Re: Is the i.MX6ULL drop-in compatible with the i.MX6UL?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Is-the-i-MX6ULL-drop-in-compatible-with-the-i-MX6UL/m-p/1235778#M169967</link>
      <description>&lt;P&gt;Hello Jay,&lt;/P&gt;&lt;P&gt;I am thinking of using 1.4V for both DDR3L and&amp;nbsp;&lt;SPAN&gt;VDD_SOC_IN&amp;nbsp;for iMX6ULL 900 MHz..&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;How did your board turn out? Did you bump into any issues?&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 24 Feb 2021 13:52:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Is-the-i-MX6ULL-drop-in-compatible-with-the-i-MX6UL/m-p/1235778#M169967</guid>
      <dc:creator>abdullahkahrama</dc:creator>
      <dc:date>2021-02-24T13:52:47Z</dc:date>
    </item>
  </channel>
</rss>