<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: SD card compatibility problem in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/SD-card-compatibility-problem/m-p/706034#M109698</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Hyobok&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;this may be signal integrity issue so one can tweak drive strength of sd signals&lt;BR /&gt;using pad control registers, like IOMUXC_SW_PAD_CTL_PAD_SD3_DATA2.&lt;BR /&gt;and in dts file one can look at entries like&lt;BR /&gt;&amp;amp;usdhc3 { &amp;nbsp;&amp;nbsp; &amp;nbsp;pinctrl-names = "default", "state_100mhz", "state_200mhz"; &lt;BR /&gt;&lt;A href="http://git.freescale.com/git/cgit.cgi/imx/linux-imx.git/tree/arch/arm/boot/dts/imx6qdl-sabreauto.dtsi?h=imx_4.1.15_2.0.0_ga&amp;amp;id=rel_imx_4.1.15_2.0.0_ga"&gt;http://git.freescale.com/git/cgit.cgi/imx/linux-imx.git/tree/arch/arm/boot/dts/imx6qdl-sabreauto.dtsi?h=imx_4.1.15_2.0.0_ga&amp;amp;id=rel_imx_4.1.15_2.0.0_ga&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sun, 27 Aug 2017 22:50:58 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2017-08-27T22:50:58Z</dc:date>
    <item>
      <title>SD card compatibility problem</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/SD-card-compatibility-problem/m-p/706033#M109697</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello.&lt;/P&gt;&lt;P&gt;I'm working on Yocto 4.1.15-1.0.0 ga release with &amp;nbsp;i.MX6 Solo and custom board.&lt;/P&gt;&lt;P&gt;Now I have SD cad compatibility problem with SD2 channel of i.MX6 Solo.&lt;/P&gt;&lt;P&gt;I have 4 SD memory cards. two of them working fine, but two are fail.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The working SD memory card was&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp;Transcend Class 10 30MB/s 200x 16GB &amp;amp;&amp;nbsp;Secure Digital 66X ULTIMA II 1GB&lt;/P&gt;&lt;P&gt;The fail SD memory card was&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp;Transcend Class 10 8GB &amp;amp;&amp;nbsp;Transcend Class 6 4GB&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It looks like low speed device is not working.&lt;/P&gt;&lt;P&gt;is there any problem in default device driver?&lt;/P&gt;&lt;P&gt;or, need I fix driver source to support it myself?&lt;/P&gt;&lt;P&gt;then where I must fix it?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I do not change any SD/MMC driver and device tree on Linux 4.1.15 from Yocto build.&lt;/P&gt;&lt;P&gt;Just enable device tree and add to support card detect GPIO pin for SD2 interface.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;please give me any idea to fix this problem.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 24 Aug 2017 13:35:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/SD-card-compatibility-problem/m-p/706033#M109697</guid>
      <dc:creator>hyobokahn</dc:creator>
      <dc:date>2017-08-24T13:35:50Z</dc:date>
    </item>
    <item>
      <title>Re: SD card compatibility problem</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/SD-card-compatibility-problem/m-p/706034#M109698</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Hyobok&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;this may be signal integrity issue so one can tweak drive strength of sd signals&lt;BR /&gt;using pad control registers, like IOMUXC_SW_PAD_CTL_PAD_SD3_DATA2.&lt;BR /&gt;and in dts file one can look at entries like&lt;BR /&gt;&amp;amp;usdhc3 { &amp;nbsp;&amp;nbsp; &amp;nbsp;pinctrl-names = "default", "state_100mhz", "state_200mhz"; &lt;BR /&gt;&lt;A href="http://git.freescale.com/git/cgit.cgi/imx/linux-imx.git/tree/arch/arm/boot/dts/imx6qdl-sabreauto.dtsi?h=imx_4.1.15_2.0.0_ga&amp;amp;id=rel_imx_4.1.15_2.0.0_ga"&gt;http://git.freescale.com/git/cgit.cgi/imx/linux-imx.git/tree/arch/arm/boot/dts/imx6qdl-sabreauto.dtsi?h=imx_4.1.15_2.0.0_ga&amp;amp;id=rel_imx_4.1.15_2.0.0_ga&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 27 Aug 2017 22:50:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/SD-card-compatibility-problem/m-p/706034#M109698</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2017-08-27T22:50:58Z</dc:date>
    </item>
  </channel>
</rss>