<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックiMX7 LPDDR3 Length Matching</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/iMX7-LPDDR3-Length-Matching/m-p/706018#M109688</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We are planing to use IMX7 processor with LPDDR3.&lt;/P&gt;&lt;P&gt;In the LPDDR3 Length Match Guideline its given as&lt;/P&gt;&lt;P&gt;"&lt;STRONG&gt;Match the signals of each byte group ± 55 mils to the strobe. Limit minimum DQS length to Clock (min) – 200 mils.If the DQS strobe is more than 200 mils shorter than Clock (min), consider manually adjusting each field of register &lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;DDR_PHY_LVL_CON0. Increment +1 for each 100 mils that the DQS trace is shorter than Clock (min)&lt;/STRONG&gt;."&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;What is the maximum "DQS Strobe" signal length that we need to maintain? In guideline they mentioned "DQS Strobe" minimum value.(i.e..Limit minimum DQS length to Clock (min) – 200 mils) but they did't talked about maximum length value. Can any one tell what is the maximum value that we need to maintain.&lt;/LI&gt;&lt;LI&gt;In guideline they mentioned if "DQS strobe is more than 200 mils shorter than Clock (min), consider manually adjusting each field of register DDR_PHY_LVL_CON0. Increment +1 for each 100 mils that the DQS trace is shorter than Clock (min).". If we followed above rule anyone faced any issue? pls confirm.&lt;/LI&gt;&lt;LI&gt;In the Reference manual did not give much details about the Register DDR_PHY_LVL_CON0. They have given as Write Level Slave DLL Code Value for Data_Slice 0 ,1,2,3.&amp;nbsp;&amp;nbsp;&amp;nbsp; Can Any one share the details of these register and its usage&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: black;"&gt;Thanks &amp;amp; Regards,&lt;BR /&gt; Pushpanathan&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 24 Aug 2017 10:23:46 GMT</pubDate>
    <dc:creator>pushpanathan</dc:creator>
    <dc:date>2017-08-24T10:23:46Z</dc:date>
    <item>
      <title>iMX7 LPDDR3 Length Matching</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX7-LPDDR3-Length-Matching/m-p/706018#M109688</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We are planing to use IMX7 processor with LPDDR3.&lt;/P&gt;&lt;P&gt;In the LPDDR3 Length Match Guideline its given as&lt;/P&gt;&lt;P&gt;"&lt;STRONG&gt;Match the signals of each byte group ± 55 mils to the strobe. Limit minimum DQS length to Clock (min) – 200 mils.If the DQS strobe is more than 200 mils shorter than Clock (min), consider manually adjusting each field of register &lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;DDR_PHY_LVL_CON0. Increment +1 for each 100 mils that the DQS trace is shorter than Clock (min)&lt;/STRONG&gt;."&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;What is the maximum "DQS Strobe" signal length that we need to maintain? In guideline they mentioned "DQS Strobe" minimum value.(i.e..Limit minimum DQS length to Clock (min) – 200 mils) but they did't talked about maximum length value. Can any one tell what is the maximum value that we need to maintain.&lt;/LI&gt;&lt;LI&gt;In guideline they mentioned if "DQS strobe is more than 200 mils shorter than Clock (min), consider manually adjusting each field of register DDR_PHY_LVL_CON0. Increment +1 for each 100 mils that the DQS trace is shorter than Clock (min).". If we followed above rule anyone faced any issue? pls confirm.&lt;/LI&gt;&lt;LI&gt;In the Reference manual did not give much details about the Register DDR_PHY_LVL_CON0. They have given as Write Level Slave DLL Code Value for Data_Slice 0 ,1,2,3.&amp;nbsp;&amp;nbsp;&amp;nbsp; Can Any one share the details of these register and its usage&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: black;"&gt;Thanks &amp;amp; Regards,&lt;BR /&gt; Pushpanathan&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 24 Aug 2017 10:23:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX7-LPDDR3-Length-Matching/m-p/706018#M109688</guid>
      <dc:creator>pushpanathan</dc:creator>
      <dc:date>2017-08-24T10:23:46Z</dc:date>
    </item>
    <item>
      <title>Re: iMX7 LPDDR3 Length Matching</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX7-LPDDR3-Length-Matching/m-p/706019#M109689</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi &lt;SPAN style="color: black;"&gt;Pushpanathan&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;according to Table 19. DDR trace routing guidelines Hardware Development Guide&lt;/P&gt;&lt;P&gt;for i.MX7Dual and 7Solo Applications Processors &lt;BR /&gt;&lt;A class="jive-link-external-small" href="https://community.nxp.com/external-link.jspa?url=http%3A%2F%2Fwww.nxp.com%2Ffiles%2F32bit%2Fdoc%2Fuser_guide%2FIMX7DSHDG.pdf" rel="nofollow" target="_blank"&gt;http://www.nxp.com/files/32bit/doc/user_guide/IMX7DSHDG.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;DQS strobe should have maximum length of Clock -10 mils&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It is based upon allocating various margins of error for each of the areas that could affect&lt;BR /&gt;DDR timing, and still provide a safety margin to ensure that DDR operations fall within the requirements of the&lt;BR /&gt;JEDEC standards. Margins of error include areas such as: Internal silicon design, variances through the pads/&lt;BR /&gt;balls, PCB design variances, variences for the LPDDR3 device.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 25 Aug 2017 22:45:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX7-LPDDR3-Length-Matching/m-p/706019#M109689</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2017-08-25T22:45:43Z</dc:date>
    </item>
  </channel>
</rss>