<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックIs INTC different from GIC( Generic interrupt controller)</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Is-INTC-different-from-GIC-Generic-interrupt-controller/m-p/705231#M109558</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi , &lt;/P&gt;&lt;P&gt;I am going through the IMX6&amp;nbsp;reference manual ,&amp;nbsp;INTC supports the 128 interrupts and it generates the wakeup signal to the CPU . My questions are as below :&lt;/P&gt;&lt;P&gt;Q1 : Is this INTC different from GIC?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Q2 &amp;nbsp;Also , i could not see the GIC in the architecture block diagram of the reference manual . I would like to understand how the GIC is interfaced with the processor. Could you please help me understand this .&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Aditya nagal&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 15 Sep 2017 12:53:54 GMT</pubDate>
    <dc:creator>adityanagal</dc:creator>
    <dc:date>2017-09-15T12:53:54Z</dc:date>
    <item>
      <title>Is INTC different from GIC( Generic interrupt controller)</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Is-INTC-different-from-GIC-Generic-interrupt-controller/m-p/705231#M109558</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi , &lt;/P&gt;&lt;P&gt;I am going through the IMX6&amp;nbsp;reference manual ,&amp;nbsp;INTC supports the 128 interrupts and it generates the wakeup signal to the CPU . My questions are as below :&lt;/P&gt;&lt;P&gt;Q1 : Is this INTC different from GIC?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Q2 &amp;nbsp;Also , i could not see the GIC in the architecture block diagram of the reference manual . I would like to understand how the GIC is interfaced with the processor. Could you please help me understand this .&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Aditya nagal&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 15 Sep 2017 12:53:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Is-INTC-different-from-GIC-Generic-interrupt-controller/m-p/705231#M109558</guid>
      <dc:creator>adityanagal</dc:creator>
      <dc:date>2017-09-15T12:53:54Z</dc:date>
    </item>
    <item>
      <title>Re: Is INTC different from GIC( Generic interrupt controller)</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Is-INTC-different-from-GIC-Generic-interrupt-controller/m-p/705232#M109559</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Aditya,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;They are not the same, the GIC is an internal module that belongs to the Cortex A processor and this is why you don't find connections in the block diagram. You can find more information about it in ARM infocenter.&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="http://infocenter.arm.com/help/index.jsp?topic=/com.arm.doc.ddi0407g/CHDHACEH.html" title="http://infocenter.arm.com/help/index.jsp?topic=/com.arm.doc.ddi0407g/CHDHACEH.html"&gt;ARM Information Center&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;On the other side the INTC is an interrupt controller just for the GPC module&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Regards,&lt;BR /&gt;Carlos&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 18 Sep 2017 19:57:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Is-INTC-different-from-GIC-Generic-interrupt-controller/m-p/705232#M109559</guid>
      <dc:creator>Carlos_Musich</dc:creator>
      <dc:date>2017-09-18T19:57:25Z</dc:date>
    </item>
  </channel>
</rss>