<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic iMX6Q interface with eMMC5.1 in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/iMX6Q-interface-with-eMMC5-1/m-p/704853#M109498</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am using iMX6Q&amp;nbsp;on my custom board. I am planning to use eMMC&amp;nbsp;5.1.&amp;nbsp;&lt;/P&gt;&lt;P&gt;The eMMC is backward compatible to eMMC&amp;nbsp;4.5 &amp;amp; eMMC 5.0 versions only. I found iMX6Q only support MMC version upto&amp;nbsp;max v4.41.&lt;/P&gt;&lt;P&gt;So just want to confirm, Can I interface iMX6Q with this eMMC and Boot my custom board from eMMC&amp;nbsp;by doing any modifications?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Ritesh&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 23 Aug 2017 07:07:37 GMT</pubDate>
    <dc:creator>riteshpatel</dc:creator>
    <dc:date>2017-08-23T07:07:37Z</dc:date>
    <item>
      <title>iMX6Q interface with eMMC5.1</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX6Q-interface-with-eMMC5-1/m-p/704853#M109498</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am using iMX6Q&amp;nbsp;on my custom board. I am planning to use eMMC&amp;nbsp;5.1.&amp;nbsp;&lt;/P&gt;&lt;P&gt;The eMMC is backward compatible to eMMC&amp;nbsp;4.5 &amp;amp; eMMC 5.0 versions only. I found iMX6Q only support MMC version upto&amp;nbsp;max v4.41.&lt;/P&gt;&lt;P&gt;So just want to confirm, Can I interface iMX6Q with this eMMC and Boot my custom board from eMMC&amp;nbsp;by doing any modifications?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Ritesh&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 23 Aug 2017 07:07:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX6Q-interface-with-eMMC5-1/m-p/704853#M109498</guid>
      <dc:creator>riteshpatel</dc:creator>
      <dc:date>2017-08-23T07:07:37Z</dc:date>
    </item>
    <item>
      <title>Re: iMX6Q interface with eMMC5.1</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX6Q-interface-with-eMMC5-1/m-p/704854#M109499</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Ritesh&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;right, iMX6Q formally only support MMC version up to v4.41, this means support for&lt;/P&gt;&lt;P&gt;full functionality defined by that version of specification. However basic read/write&lt;/P&gt;&lt;P&gt;operations may be supported with more newer versions like eMMC&amp;nbsp;4.5 &amp;amp; eMMC 5.0 versions.&lt;/P&gt;&lt;P&gt;As eMMC&amp;nbsp;5.1 is compatible with these versions, seems it will work fine with it too.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 23 Aug 2017 07:31:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX6Q-interface-with-eMMC5-1/m-p/704854#M109499</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2017-08-23T07:31:27Z</dc:date>
    </item>
    <item>
      <title>Re: iMX6Q interface with eMMC5.1</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX6Q-interface-with-eMMC5-1/m-p/704855#M109500</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Igor,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for the Quick&amp;nbsp;response.&lt;/P&gt;&lt;P&gt;That means the read/write operations can be possible between iMX6Q (supports up to&amp;nbsp;ver4.4/4.41) and eMMC&amp;nbsp;5.1 with backward compatibility ver 4.5 &amp;amp; ver 5.0. But the booting the iMX6Q may not be possible with eMMC&amp;nbsp;5.1/5.0/4.5. Please correct if wrong.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 23 Aug 2017 08:34:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX6Q-interface-with-eMMC5-1/m-p/704855#M109500</guid>
      <dc:creator>riteshpatel</dc:creator>
      <dc:date>2017-08-23T08:34:22Z</dc:date>
    </item>
    <item>
      <title>Re: iMX6Q interface with eMMC5.1</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX6Q-interface-with-eMMC5-1/m-p/704856#M109501</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Ritesh&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;right, it should support basic read/write operations and also booting, please look at :&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-332187"&gt;https://community.nxp.com/docs/DOC-332187&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 23 Aug 2017 11:18:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX6Q-interface-with-eMMC5-1/m-p/704856#M109501</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2017-08-23T11:18:31Z</dc:date>
    </item>
  </channel>
</rss>