<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: QT support for IMX7</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/QT-support-for-IMX7/m-p/703757#M109335</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Gopinath&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;please check&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://lists.yoctoproject.org/pipermail/meta-freescale/2016-September/019110.html" title="https://lists.yoctoproject.org/pipermail/meta-freescale/2016-September/019110.html"&gt;[meta-freescale] [meta-fsl-arm PATCH v3 17/17] qtbase: Enable support for i.MX SoCs with PXP&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;As for nxp bsps, attached Yocto Guide Table 1. i.MX Yocto project images states:&lt;/P&gt;&lt;P&gt;opensource Qt 5 image. These images are only supported for i.MX SoC with hardware graphics.&lt;/P&gt;&lt;P&gt;They are not supported on the i.MX 6UltraLite, i.MX 6UltraLiteLite, and i.MX 7Dual.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 11 Oct 2017 23:25:15 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2017-10-11T23:25:15Z</dc:date>
    <item>
      <title>QT support for IMX7</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/QT-support-for-IMX7/m-p/703756#M109334</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Everyone,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am working on QT support in IMX7. From release notes, I understand that &lt;STRONG&gt;"QT&amp;nbsp;is not supported on i.MX 7Dual and It works on X11 backend only but is not a supported feature".&amp;nbsp;&lt;/STRONG&gt;Now I want to enable support for QT in yocto build. Any suggestion for this.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So far I have tried to build QT by, "bitbake fsl-image-qt5" command. But I am getting below error.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;NOTE: Runtime target '\' is unbuildable, removing...&lt;BR /&gt;Missing or unbuildable dependency chain was: ['\\']&lt;BR /&gt;ERROR: Required build target 'fsl-image-qt5' has no buildable providers.&lt;BR /&gt;Missing or unbuildable dependency chain was: ['fsl-image-qt5', '\\']&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can anyone please help me on this?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Gopinath S&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 11 Oct 2017 13:43:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/QT-support-for-IMX7/m-p/703756#M109334</guid>
      <dc:creator>gopinathsriniva</dc:creator>
      <dc:date>2017-10-11T13:43:30Z</dc:date>
    </item>
    <item>
      <title>Re: QT support for IMX7</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/QT-support-for-IMX7/m-p/703757#M109335</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Gopinath&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;please check&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://lists.yoctoproject.org/pipermail/meta-freescale/2016-September/019110.html" title="https://lists.yoctoproject.org/pipermail/meta-freescale/2016-September/019110.html"&gt;[meta-freescale] [meta-fsl-arm PATCH v3 17/17] qtbase: Enable support for i.MX SoCs with PXP&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;As for nxp bsps, attached Yocto Guide Table 1. i.MX Yocto project images states:&lt;/P&gt;&lt;P&gt;opensource Qt 5 image. These images are only supported for i.MX SoC with hardware graphics.&lt;/P&gt;&lt;P&gt;They are not supported on the i.MX 6UltraLite, i.MX 6UltraLiteLite, and i.MX 7Dual.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 11 Oct 2017 23:25:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/QT-support-for-IMX7/m-p/703757#M109335</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2017-10-11T23:25:15Z</dc:date>
    </item>
  </channel>
</rss>