<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: IMX6Q adding ECSPI1 driver in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/IMX6Q-adding-ECSPI1-driver/m-p/703731#M109333</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi yong,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;the commented lines are the ones that you are adding and the ones that causes the problem?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;If this is the case then how are you handling the CS? I can see that you are commenting out the pin that works as chip select.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Carlos&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 06 Sep 2017 23:46:58 GMT</pubDate>
    <dc:creator>Carlos_Musich</dc:creator>
    <dc:date>2017-09-06T23:46:58Z</dc:date>
    <item>
      <title>IMX6Q adding ECSPI1 driver</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6Q-adding-ECSPI1-driver/m-p/703730#M109332</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Recently I am trying to get Linux Kernel SPI driver working with ECSPI1 on IMX6Q. I have successfully implemented the driver on ECSPI3 and passed the close-loop SPI test. The driver and device tree are matching well with a character device node at /dev/spidev32766.0. However when I am adding a new SPI device node in file &amp;lt;imx6qdl-sabreauto.dtsi&amp;gt; with the following modification:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;amp;ecspi1 {&lt;BR /&gt; fsl,spi-num-chipselects = &amp;lt;1&amp;gt;;&lt;BR /&gt; cs-gpios = &amp;lt;&amp;amp;gpio3 19 0&amp;gt;;&lt;BR /&gt; //cs-gpios = &amp;lt;0&amp;gt;;&lt;BR /&gt; pinctrl-names = "default";&lt;BR /&gt; pinctrl-0 = &amp;lt;&amp;amp;pinctrl_ecspi1_1 &amp;amp;pinctrl_ecspi1_cs_1&amp;gt;;&lt;BR /&gt; //pinctrl-0 = &amp;lt;&amp;amp;pinctrl_ecspi1_1&amp;gt;;&lt;BR /&gt; status = "okay";&lt;BR /&gt; spidev1: spi@0 {&lt;BR /&gt; compatible = "spidev";&lt;BR /&gt; reg = &amp;lt;0&amp;gt;;&lt;BR /&gt; spi-max-frequency = &amp;lt;1000000&amp;gt;;&lt;BR /&gt; };&lt;BR /&gt;};&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am able to create a new character device node at&amp;nbsp;&lt;SPAN&gt;/dev/spidev32765.0. But there is data sending out when doing the close-loop test.&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;What could I possibly miss? Any help would be appreciated. Thanks!&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 22 Aug 2017 10:10:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6Q-adding-ECSPI1-driver/m-p/703730#M109332</guid>
      <dc:creator>yongggg</dc:creator>
      <dc:date>2017-08-22T10:10:26Z</dc:date>
    </item>
    <item>
      <title>Re: IMX6Q adding ECSPI1 driver</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6Q-adding-ECSPI1-driver/m-p/703731#M109333</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi yong,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;the commented lines are the ones that you are adding and the ones that causes the problem?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;If this is the case then how are you handling the CS? I can see that you are commenting out the pin that works as chip select.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Carlos&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 06 Sep 2017 23:46:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6Q-adding-ECSPI1-driver/m-p/703731#M109333</guid>
      <dc:creator>Carlos_Musich</dc:creator>
      <dc:date>2017-09-06T23:46:58Z</dc:date>
    </item>
  </channel>
</rss>