<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: i.MX287 problem with NAND</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-MX287-problem-with-NAND/m-p/703303#M109280</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&amp;nbsp; The boot console code 0x80508002 means "Unable to find FCB".&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;Some details about the FCB may be found in the i.MX28 Reference Manual, &lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;chapter 12 (Boot Modes). &lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; The code 0x80502008 means the following: if the boot ROM is unable to boot from &lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;the device, indicated by the boot mode (NAND), then it falls back to the USB interface. &lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;This error code indicates that the USB boot failed as well. &lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&amp;nbsp; Also, please look at the following thread. &lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-95515"&gt;https://community.nxp.com/docs/DOC-95515&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Yuri&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 11 Oct 2017 09:34:03 GMT</pubDate>
    <dc:creator>Yuri</dc:creator>
    <dc:date>2017-10-11T09:34:03Z</dc:date>
    <item>
      <title>i.MX287 problem with NAND</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX287-problem-with-NAND/m-p/703302#M109279</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all,&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We're developing custom device based on MCIMX287CVM4B (TAIW) and Macronix NAND MX30LF2G18AC. It's perfectly working with U-Boot 2014.10 and 3.18 linux kernel.&lt;/P&gt;&lt;P&gt;Nowadays our suppliers&amp;nbsp;instead of Macronix brought an analog Winbond W29N02GVBIAA. But when testing the devices it turned out that they are switching on non-stably. In the same time the replacement of Winbond with Macronix solving this problem.&amp;nbsp;&lt;/P&gt;&lt;P&gt;I connected to the debug uart and saw the error codes 0x80508002 and&amp;nbsp;&amp;nbsp;&lt;SPAN&gt;0x80502008. Then I connected to the USB and load and run U-Boot from RAM. U-boot confirmed that all OK, then its started booting kernel and&amp;nbsp;system. When I did soft-reboot, its&amp;nbsp;again expected the download from usb.&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;What could be the problem? What should I look for?&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Thank you for your cooperation.&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 11 Oct 2017 07:17:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX287-problem-with-NAND/m-p/703302#M109279</guid>
      <dc:creator>iuncuim</dc:creator>
      <dc:date>2017-10-11T07:17:17Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX287 problem with NAND</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX287-problem-with-NAND/m-p/703303#M109280</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&amp;nbsp; The boot console code 0x80508002 means "Unable to find FCB".&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;Some details about the FCB may be found in the i.MX28 Reference Manual, &lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;chapter 12 (Boot Modes). &lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; The code 0x80502008 means the following: if the boot ROM is unable to boot from &lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;the device, indicated by the boot mode (NAND), then it falls back to the USB interface. &lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;This error code indicates that the USB boot failed as well. &lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&amp;nbsp; Also, please look at the following thread. &lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-95515"&gt;https://community.nxp.com/docs/DOC-95515&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Yuri&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 11 Oct 2017 09:34:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX287-problem-with-NAND/m-p/703303#M109280</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2017-10-11T09:34:03Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX287 problem with NAND</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX287-problem-with-NAND/m-p/703304#M109281</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you for your answer. I&amp;nbsp;read about error codes and what they means. Can you give me your contacts (e-mail, skype, telegram, whatsapp)? I would try to explain the problem in our&amp;nbsp;native language&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 11 Oct 2017 10:28:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX287-problem-with-NAND/m-p/703304#M109281</guid>
      <dc:creator>iuncuim</dc:creator>
      <dc:date>2017-10-11T10:28:25Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX287 problem with NAND</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX287-problem-with-NAND/m-p/703305#M109282</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; You may try to create request on native language.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://www.nxp.com/support/support:SUPPORTHOME?tid=sbmenu" title="https://www.nxp.com/support/support:SUPPORTHOME?tid=sbmenu"&gt;Support|NXP&lt;/A&gt;&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Yuri.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 12 Oct 2017 08:42:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX287-problem-with-NAND/m-p/703305#M109282</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2017-10-12T08:42:25Z</dc:date>
    </item>
  </channel>
</rss>