<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: linux porting in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/linux-porting/m-p/702622#M109171</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Ok i will send it to you soon&lt;/P&gt;&lt;P&gt;Byee&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 19 Oct 2017 17:03:06 GMT</pubDate>
    <dc:creator>saida</dc:creator>
    <dc:date>2017-10-19T17:03:06Z</dc:date>
    <item>
      <title>linux porting</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/linux-porting/m-p/702617#M109166</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;hi&lt;/P&gt;&lt;P&gt;I have a customized imxdl hardware board where extra devices are added and pin muxing also different&amp;nbsp; from sabresd board&lt;/P&gt;&lt;P&gt;i am able to port u-boot,linux kernel and rootfile system with sabresd board which i purchased&lt;/P&gt;&lt;P&gt;in my custom board i am using uart3 and i chaned it in u-boot UART3_BASE ans CONSOLE is ttymxc2&lt;/P&gt;&lt;P&gt;so u-boot is working but kernel is not booting (i am using imx6dl-sabresd.dtb file for kernel booting which is in kernel)&lt;/P&gt;&lt;P&gt;it is stopping at 'Starting Kernel'&lt;/P&gt;&lt;P&gt;no further console messages&lt;/P&gt;&lt;P&gt;what could be the problem&lt;/P&gt;&lt;P&gt;thanks and regards&lt;/P&gt;&lt;P&gt;saida&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 11 Oct 2017 08:46:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/linux-porting/m-p/702617#M109166</guid>
      <dc:creator>saida</dc:creator>
      <dc:date>2017-10-11T08:46:17Z</dc:date>
    </item>
    <item>
      <title>Re: linux porting</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/linux-porting/m-p/702618#M109167</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;You need to update u-boot options with new console and make sure that Linux kernel itself supports it.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Victor&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 13 Oct 2017 04:45:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/linux-porting/m-p/702618#M109167</guid>
      <dc:creator>b36401</dc:creator>
      <dc:date>2017-10-13T04:45:50Z</dc:date>
    </item>
    <item>
      <title>Re: linux porting</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/linux-porting/m-p/702619#M109168</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;A _jive_internal="true" data-content-finding="Community" data-userid="230965" data-username="saida" href="https://community.nxp.com/people/saida"&gt;&lt;SPAN style="color: #0066cc; text-decoration: underline;"&gt;Saida S&lt;/SPAN&gt;&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Have you configed the gpio for uart3 correctly in the dts?if so ,you can do the test(communicate with the PC by read/write the uart)&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 13 Oct 2017 09:29:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/linux-porting/m-p/702619#M109168</guid>
      <dc:creator>jingyangxie</dc:creator>
      <dc:date>2017-10-13T09:29:12Z</dc:date>
    </item>
    <item>
      <title>Re: linux porting</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/linux-porting/m-p/702620#M109169</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you for your replay&lt;/P&gt;&lt;P&gt;I changed gpio pins for UART 3 in dtsi file and it is updated in dtb file after build also&lt;/P&gt;&lt;P&gt;But still it's not working. Where this UART 3 initialized in Linux ? I am debugging through source code also , if you have any clues plZ share it i will try and come back to you&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you very much&lt;/P&gt;&lt;P&gt;Regards&amp;nbsp;&lt;/P&gt;&lt;P&gt;Saida&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 16 Oct 2017 16:21:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/linux-porting/m-p/702620#M109169</guid>
      <dc:creator>saida</dc:creator>
      <dc:date>2017-10-16T16:21:48Z</dc:date>
    </item>
    <item>
      <title>Re: linux porting</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/linux-porting/m-p/702621#M109170</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;the whole uarts will be initialized when enabled in dts.for imx,the uart driver is in /driver/tty/serial/imx.c.you can refer the file for details.or can you give the start massage of your board?I want to know more details.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 17 Oct 2017 07:21:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/linux-porting/m-p/702621#M109170</guid>
      <dc:creator>jingyangxie</dc:creator>
      <dc:date>2017-10-17T07:21:59Z</dc:date>
    </item>
    <item>
      <title>Re: linux porting</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/linux-porting/m-p/702622#M109171</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Ok i will send it to you soon&lt;/P&gt;&lt;P&gt;Byee&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 19 Oct 2017 17:03:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/linux-porting/m-p/702622#M109171</guid>
      <dc:creator>saida</dc:creator>
      <dc:date>2017-10-19T17:03:06Z</dc:date>
    </item>
  </channel>
</rss>