<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Boot problem with u-boot sdk (imx6qsabresd)</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Boot-problem-with-u-boot-sdk-imx6qsabresd/m-p/702466#M109148</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Giray&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;also may be useful to check Linux Guide for programming images included in&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://www.nxp.com/webapp/Download?colCode=L4.9.11_1.0.0_LINUX_DOCS&amp;amp;Parent_nodeId=1337699481071706174845&amp;amp;Parent_pageType=product&amp;amp;Parent_nodeId=1337699481071706174845&amp;amp;Parent_pageType=product" title="https://www.nxp.com/webapp/Download?colCode=L4.9.11_1.0.0_LINUX_DOCS&amp;amp;Parent_nodeId=1337699481071706174845&amp;amp;Parent_pageType=product&amp;amp;Parent_nodeId=1337699481071706174845&amp;amp;Parent_pageType=product"&gt;https://www.nxp.com/webapp/Download?colCode=L4.9.11_1.0.0_LINUX_DOCS&amp;amp;Parent_nodeId=1337699481071706174845&amp;amp;Parent_pageTyp…&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;sdcard image&lt;/EM&gt; includes already uboot, so writing the "u-boot.imx" file on step 2&lt;/P&gt;&lt;P&gt;overwrites original image uboot.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 10 Oct 2017 23:09:41 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2017-10-10T23:09:41Z</dc:date>
    <item>
      <title>Boot problem with u-boot sdk (imx6qsabresd)</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Boot-problem-with-u-boot-sdk-imx6qsabresd/m-p/702464#M109146</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello all.&lt;/P&gt;&lt;P&gt;I am working to build a custom bootloader by using SDK. I have achieved to boot the custom board with only using the "u-boot.imx" inside the sdcard. However, when I try to write the "u-boot.imx" on a partitioned sdcard that includes the image that I built previously, the system uses the bootloader which is included the image itself, not the one that I have created using the SDK.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The procedure that I am following:&lt;/P&gt;&lt;P&gt;1.Writing the image on the sdcard using the "$ &lt;EM&gt;sudo dd if=&amp;lt;.sdcard image&amp;gt; of=/dev/sdb bs=1M&lt;/EM&gt;" command.&lt;/P&gt;&lt;P&gt;2.Writing the "u-boot.imx" file on the sdcard using the "$ &lt;EM&gt;sudo dd if=u-boot.imx of=/dev/sdb1 bs=1M seek=2 conv=fsync&lt;/EM&gt;"&lt;/P&gt;&lt;P&gt;command.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp; &amp;nbsp; (Additional question: The board does not boot without adding the "seek" part of the command. What is the reason &amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;of this? I will be more than happy, if you answer it.)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;(I try to write the "u-boot.imx" on the first partition of the sdcard to avoid deleting the second partition.)&lt;/P&gt;&lt;P&gt;3.Try to boot it using the board.&lt;/P&gt;&lt;P&gt;4.Board uses the original u-boot (that is included inside the image itself) not the one that I have created using the SDK. I want to boot it with the SDK one.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;(The date of compilation of the u-boot is Oct 03 2017 when I boot the device. I created the SDK one on Oct 09 &amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;2017. That is how I am telling it is using the other one. I do not know this is the correct way to tell it.)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I tried numerous solutions to solve this issue. However, none of them worked.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Many thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 10 Oct 2017 13:05:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Boot-problem-with-u-boot-sdk-imx6qsabresd/m-p/702464#M109146</guid>
      <dc:creator>gkt</dc:creator>
      <dc:date>2017-10-10T13:05:20Z</dc:date>
    </item>
    <item>
      <title>Re: Boot problem with u-boot sdk (imx6qsabresd)</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Boot-problem-with-u-boot-sdk-imx6qsabresd/m-p/702465#M109147</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Giray,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please try the following command:&lt;BR /&gt;&amp;nbsp;&amp;nbsp; $ sudo dd if=u-boot.imx of=/dev/sdX bs=1K seek=1; sync&lt;/P&gt;&lt;P&gt;Remember to replace sdX with the correct partition mounted in your PC (possible sdb).&lt;BR /&gt;&lt;BR /&gt;Thanks!&lt;BR /&gt;Vanessa&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 10 Oct 2017 16:51:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Boot-problem-with-u-boot-sdk-imx6qsabresd/m-p/702465#M109147</guid>
      <dc:creator>vanessa_maegima</dc:creator>
      <dc:date>2017-10-10T16:51:30Z</dc:date>
    </item>
    <item>
      <title>Re: Boot problem with u-boot sdk (imx6qsabresd)</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Boot-problem-with-u-boot-sdk-imx6qsabresd/m-p/702466#M109148</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Giray&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;also may be useful to check Linux Guide for programming images included in&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://www.nxp.com/webapp/Download?colCode=L4.9.11_1.0.0_LINUX_DOCS&amp;amp;Parent_nodeId=1337699481071706174845&amp;amp;Parent_pageType=product&amp;amp;Parent_nodeId=1337699481071706174845&amp;amp;Parent_pageType=product" title="https://www.nxp.com/webapp/Download?colCode=L4.9.11_1.0.0_LINUX_DOCS&amp;amp;Parent_nodeId=1337699481071706174845&amp;amp;Parent_pageType=product&amp;amp;Parent_nodeId=1337699481071706174845&amp;amp;Parent_pageType=product"&gt;https://www.nxp.com/webapp/Download?colCode=L4.9.11_1.0.0_LINUX_DOCS&amp;amp;Parent_nodeId=1337699481071706174845&amp;amp;Parent_pageTyp…&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;sdcard image&lt;/EM&gt; includes already uboot, so writing the "u-boot.imx" file on step 2&lt;/P&gt;&lt;P&gt;overwrites original image uboot.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 10 Oct 2017 23:09:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Boot-problem-with-u-boot-sdk-imx6qsabresd/m-p/702466#M109148</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2017-10-10T23:09:41Z</dc:date>
    </item>
  </channel>
</rss>