<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processorsのトピックi.MX53 boot on SD Card</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-MX53-boot-on-SD-Card/m-p/200140#M10912</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have developped an i.MX53 board with an SD Card interface.&lt;/P&gt;&lt;P&gt;U-boot runs fine at startup. I can load Linux kernel in RAM and start the kernel. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The problem is when the kernel trys to mount the rootfs, the SD Card was not detected.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I try to boot the QSB board with my SD Card&amp;nbsp; and it's run fine. (u-boot ok, kernel and rootfs ok, Loging ok )&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I don't know where to search. My board uses the same hardware for th SD Card interface, same OSC (24MHz), 1GB of RAM (actually 512MB detected but it's normal)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The only thing is the SD Card doesn't reply to any command. (CMD0 and others )&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can someone please help me ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Kernel start log :&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Uncompressing Linux... done, booting the kernel.&lt;/P&gt;&lt;P&gt;Booting Linux on physical CPU 0&lt;/P&gt;&lt;P&gt;Linux version 3.3.2-ideb0 (nicolas@gits) (gcc version 4.7.1 20120531 (prerelease) (crosstool-NG linaro-1.13.1-2012.06-20120625 - Linaro GCC 2012.06) ) #63 Tue Sep 25 15:29:41 CEST 2012&lt;/P&gt;&lt;P&gt;CPU: ARMv7 Processor [412fc085] revision 5 (ARMv7), cr=10c53c7d&lt;/P&gt;&lt;P&gt;CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache&lt;/P&gt;&lt;P&gt;Machine: AIM MX53 iDEB0 Board&lt;/P&gt;&lt;P&gt;Ignoring RAM at b0000000-cfffffff (vmalloc region overlap).&lt;/P&gt;&lt;P&gt;Memory policy: ECC disabled, Data cache writeback&lt;/P&gt;&lt;P&gt;On node 0 totalpages: 131072&lt;/P&gt;&lt;P&gt;free_area_init_node: node 0, pgdat c02e5708, node_mem_map c0301000&lt;/P&gt;&lt;P&gt;&amp;nbsp; Normal zone: 1024 pages used for memmap&lt;/P&gt;&lt;P&gt;&amp;nbsp; Normal zone: 0 pages reserved&lt;/P&gt;&lt;P&gt;&amp;nbsp; Normal zone: 130048 pages, LIFO batch:31&lt;/P&gt;&lt;P&gt;pcpu-alloc: s0 r0 d32768 u32768 alloc=1*32768&lt;/P&gt;&lt;P&gt;pcpu-alloc: [0] 0 &lt;/P&gt;&lt;P&gt;Built 1 zonelists in Zone order, mobility grouping on.&amp;nbsp; Total pages: 130048&lt;/P&gt;&lt;P&gt;Kernel command line: noinitrd console=ttymxc0,115200 debug ip=dhcp root=/dev/mmcblk0p1 rw rootwait init=/sbin/init&lt;/P&gt;&lt;P&gt;PID hash table entries: 2048 (order: 1, 8192 bytes)&lt;/P&gt;&lt;P&gt;Dentry cache hash table entries: 65536 (order: 6, 262144 bytes)&lt;/P&gt;&lt;P&gt;Inode-cache hash table entries: 32768 (order: 5, 131072 bytes)&lt;/P&gt;&lt;P&gt;Memory: 512MB = 512MB total&lt;/P&gt;&lt;P&gt;Memory: 516672k/516672k available, 7616k reserved, 0K highmem&lt;/P&gt;&lt;P&gt;Virtual kernel memory layout:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; vector&amp;nbsp; : 0xffff0000 - 0xffff1000&amp;nbsp;&amp;nbsp; (&amp;nbsp;&amp;nbsp; 4 kB)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; fixmap&amp;nbsp; : 0xfff00000 - 0xfffe0000&amp;nbsp;&amp;nbsp; ( 896 kB)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; vmalloc : 0xe0800000 - 0xff000000&amp;nbsp;&amp;nbsp; ( 488 MB)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; lowmem&amp;nbsp; : 0xc0000000 - 0xe0000000&amp;nbsp;&amp;nbsp; ( 512 MB)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; modules : 0xbf000000 - 0xc0000000&amp;nbsp;&amp;nbsp; (&amp;nbsp; 16 MB)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; .text : 0xc0008000 - 0xc02b9000&amp;nbsp;&amp;nbsp; (2756 kB)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; .init : 0xc02b9000 - 0xc02d1000&amp;nbsp;&amp;nbsp; (&amp;nbsp; 96 kB)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; .data : 0xc02d2000 - 0xc02e5d20&amp;nbsp;&amp;nbsp; (&amp;nbsp; 80 kB)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; .bss : 0xc02e5d44 - 0xc03002ac&amp;nbsp;&amp;nbsp; ( 106 kB)&lt;/P&gt;&lt;P&gt;SLUB: Genslabs=11, HWalign=64, Order=0-3, MinObjects=0, CPUs=1, Nodes=1&lt;/P&gt;&lt;P&gt;NR_IRQS:400 nr_irqs:400 400&lt;/P&gt;&lt;P&gt;TrustZone Interrupt Controller (TZIC) initialized&lt;/P&gt;&lt;P&gt;CPU identified as i.MX53, silicon rev 2.1&lt;/P&gt;&lt;P&gt;sched_clock: 32 bits at 66MHz, resolution 15ns, wraps every 64424ms&lt;/P&gt;&lt;P&gt;Console: colour dummy device 80x30&lt;/P&gt;&lt;P&gt;Calibrating delay loop... 795.44 BogoMIPS (lpj=3977216)&lt;/P&gt;&lt;P&gt;pid_max: default: 32768 minimum: 301&lt;/P&gt;&lt;P&gt;Mount-cache hash table entries: 512&lt;/P&gt;&lt;P&gt;CPU: Testing write buffer coherency: ok&lt;/P&gt;&lt;P&gt;hw perfevents: enabled with ARMv7 Cortex-A8 PMU driver, 5 counters available&lt;/P&gt;&lt;P&gt;Setting up static identity map for 0x7020a7b0 - 0x7020a808&lt;/P&gt;&lt;P&gt;gpiochip_add: registered GPIOs 0 to 31 on device: imx31-gpio.0&lt;/P&gt;&lt;P&gt;gpiochip_add: registered GPIOs 32 to 63 on device: imx31-gpio.1&lt;/P&gt;&lt;P&gt;gpiochip_add: registered GPIOs 64 to 95 on device: imx31-gpio.2&lt;/P&gt;&lt;P&gt;gpiochip_add: registered GPIOs 96 to 127 on device: imx31-gpio.3&lt;/P&gt;&lt;P&gt;gpiochip_add: registered GPIOs 128 to 159 on device: imx31-gpio.4&lt;/P&gt;&lt;P&gt;gpiochip_add: registered GPIOs 160 to 191 on device: imx31-gpio.5&lt;/P&gt;&lt;P&gt;gpiochip_add: registered GPIOs 192 to 223 on device: imx31-gpio.6&lt;/P&gt;&lt;P&gt;hw-breakpoint: debug architecture 0x4 unsupported.&lt;/P&gt;&lt;P&gt;bio: create slab &amp;lt;bio-0&amp;gt; at 0&lt;/P&gt;&lt;P&gt;SCSI subsystem initialized&lt;/P&gt;&lt;P&gt;Switching to clocksource mxc_timer1&lt;/P&gt;&lt;P&gt;i.MXC CPU frequency driver&lt;/P&gt;&lt;P&gt;msgmni has been set to 1009&lt;/P&gt;&lt;P&gt;Block layer SCSI generic (bsg) driver version 0.4 loaded (major 254)&lt;/P&gt;&lt;P&gt;io scheduler noop registered&lt;/P&gt;&lt;P&gt;io scheduler deadline registered&lt;/P&gt;&lt;P&gt;io scheduler cfq registered (default)&lt;/P&gt;&lt;P&gt;Serial: IMX driver&lt;/P&gt;&lt;P&gt;imx21-uart.0: ttymxc0 at MMIO 0x53fbc000 (irq = 31) is a IMX&lt;/P&gt;&lt;P&gt;console [ttymxc0] enabled&lt;/P&gt;&lt;P&gt;imx21-uart.1: ttymxc1 at MMIO 0x53fc0000 (irq = 32) is a IMX&lt;/P&gt;&lt;P&gt;imx21-uart.3: ttymxc3 at MMIO 0x53ff0000 (irq = 13) is a IMX&lt;/P&gt;&lt;P&gt;imx21-uart.4: ttymxc4 at MMIO 0x63f90000 (irq = 86) is a IMX&lt;/P&gt;&lt;P&gt;loop: module loaded&lt;/P&gt;&lt;P&gt;i2c /dev entries driver&lt;/P&gt;&lt;P&gt;sdhci: Secure Digital Host Controller Interface driver&lt;/P&gt;&lt;P&gt;sdhci: Copyright(c) Pierre Ossman&lt;/P&gt;&lt;P&gt;sdhci-pltfm: SDHCI platform and OF driver helper&lt;/P&gt;&lt;P&gt;mmc0: SDHCI controller on sdhci-esdhc-imx53.0 [sdhci-esdhc-imx53.0] using DMA&lt;/P&gt;&lt;P&gt;VFP support v0.3: implementor 41 architecture 3 part 30 variant c rev 2&lt;/P&gt;&lt;P&gt;Waiting for root device /dev/mmcblk0p1...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;regards&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;Nicolas K&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 25 Sep 2012 14:40:47 GMT</pubDate>
    <dc:creator>nicolask</dc:creator>
    <dc:date>2012-09-25T14:40:47Z</dc:date>
    <item>
      <title>i.MX53 boot on SD Card</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX53-boot-on-SD-Card/m-p/200140#M10912</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have developped an i.MX53 board with an SD Card interface.&lt;/P&gt;&lt;P&gt;U-boot runs fine at startup. I can load Linux kernel in RAM and start the kernel. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The problem is when the kernel trys to mount the rootfs, the SD Card was not detected.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I try to boot the QSB board with my SD Card&amp;nbsp; and it's run fine. (u-boot ok, kernel and rootfs ok, Loging ok )&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I don't know where to search. My board uses the same hardware for th SD Card interface, same OSC (24MHz), 1GB of RAM (actually 512MB detected but it's normal)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The only thing is the SD Card doesn't reply to any command. (CMD0 and others )&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can someone please help me ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Kernel start log :&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Uncompressing Linux... done, booting the kernel.&lt;/P&gt;&lt;P&gt;Booting Linux on physical CPU 0&lt;/P&gt;&lt;P&gt;Linux version 3.3.2-ideb0 (nicolas@gits) (gcc version 4.7.1 20120531 (prerelease) (crosstool-NG linaro-1.13.1-2012.06-20120625 - Linaro GCC 2012.06) ) #63 Tue Sep 25 15:29:41 CEST 2012&lt;/P&gt;&lt;P&gt;CPU: ARMv7 Processor [412fc085] revision 5 (ARMv7), cr=10c53c7d&lt;/P&gt;&lt;P&gt;CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache&lt;/P&gt;&lt;P&gt;Machine: AIM MX53 iDEB0 Board&lt;/P&gt;&lt;P&gt;Ignoring RAM at b0000000-cfffffff (vmalloc region overlap).&lt;/P&gt;&lt;P&gt;Memory policy: ECC disabled, Data cache writeback&lt;/P&gt;&lt;P&gt;On node 0 totalpages: 131072&lt;/P&gt;&lt;P&gt;free_area_init_node: node 0, pgdat c02e5708, node_mem_map c0301000&lt;/P&gt;&lt;P&gt;&amp;nbsp; Normal zone: 1024 pages used for memmap&lt;/P&gt;&lt;P&gt;&amp;nbsp; Normal zone: 0 pages reserved&lt;/P&gt;&lt;P&gt;&amp;nbsp; Normal zone: 130048 pages, LIFO batch:31&lt;/P&gt;&lt;P&gt;pcpu-alloc: s0 r0 d32768 u32768 alloc=1*32768&lt;/P&gt;&lt;P&gt;pcpu-alloc: [0] 0 &lt;/P&gt;&lt;P&gt;Built 1 zonelists in Zone order, mobility grouping on.&amp;nbsp; Total pages: 130048&lt;/P&gt;&lt;P&gt;Kernel command line: noinitrd console=ttymxc0,115200 debug ip=dhcp root=/dev/mmcblk0p1 rw rootwait init=/sbin/init&lt;/P&gt;&lt;P&gt;PID hash table entries: 2048 (order: 1, 8192 bytes)&lt;/P&gt;&lt;P&gt;Dentry cache hash table entries: 65536 (order: 6, 262144 bytes)&lt;/P&gt;&lt;P&gt;Inode-cache hash table entries: 32768 (order: 5, 131072 bytes)&lt;/P&gt;&lt;P&gt;Memory: 512MB = 512MB total&lt;/P&gt;&lt;P&gt;Memory: 516672k/516672k available, 7616k reserved, 0K highmem&lt;/P&gt;&lt;P&gt;Virtual kernel memory layout:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; vector&amp;nbsp; : 0xffff0000 - 0xffff1000&amp;nbsp;&amp;nbsp; (&amp;nbsp;&amp;nbsp; 4 kB)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; fixmap&amp;nbsp; : 0xfff00000 - 0xfffe0000&amp;nbsp;&amp;nbsp; ( 896 kB)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; vmalloc : 0xe0800000 - 0xff000000&amp;nbsp;&amp;nbsp; ( 488 MB)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; lowmem&amp;nbsp; : 0xc0000000 - 0xe0000000&amp;nbsp;&amp;nbsp; ( 512 MB)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; modules : 0xbf000000 - 0xc0000000&amp;nbsp;&amp;nbsp; (&amp;nbsp; 16 MB)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; .text : 0xc0008000 - 0xc02b9000&amp;nbsp;&amp;nbsp; (2756 kB)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; .init : 0xc02b9000 - 0xc02d1000&amp;nbsp;&amp;nbsp; (&amp;nbsp; 96 kB)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; .data : 0xc02d2000 - 0xc02e5d20&amp;nbsp;&amp;nbsp; (&amp;nbsp; 80 kB)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; .bss : 0xc02e5d44 - 0xc03002ac&amp;nbsp;&amp;nbsp; ( 106 kB)&lt;/P&gt;&lt;P&gt;SLUB: Genslabs=11, HWalign=64, Order=0-3, MinObjects=0, CPUs=1, Nodes=1&lt;/P&gt;&lt;P&gt;NR_IRQS:400 nr_irqs:400 400&lt;/P&gt;&lt;P&gt;TrustZone Interrupt Controller (TZIC) initialized&lt;/P&gt;&lt;P&gt;CPU identified as i.MX53, silicon rev 2.1&lt;/P&gt;&lt;P&gt;sched_clock: 32 bits at 66MHz, resolution 15ns, wraps every 64424ms&lt;/P&gt;&lt;P&gt;Console: colour dummy device 80x30&lt;/P&gt;&lt;P&gt;Calibrating delay loop... 795.44 BogoMIPS (lpj=3977216)&lt;/P&gt;&lt;P&gt;pid_max: default: 32768 minimum: 301&lt;/P&gt;&lt;P&gt;Mount-cache hash table entries: 512&lt;/P&gt;&lt;P&gt;CPU: Testing write buffer coherency: ok&lt;/P&gt;&lt;P&gt;hw perfevents: enabled with ARMv7 Cortex-A8 PMU driver, 5 counters available&lt;/P&gt;&lt;P&gt;Setting up static identity map for 0x7020a7b0 - 0x7020a808&lt;/P&gt;&lt;P&gt;gpiochip_add: registered GPIOs 0 to 31 on device: imx31-gpio.0&lt;/P&gt;&lt;P&gt;gpiochip_add: registered GPIOs 32 to 63 on device: imx31-gpio.1&lt;/P&gt;&lt;P&gt;gpiochip_add: registered GPIOs 64 to 95 on device: imx31-gpio.2&lt;/P&gt;&lt;P&gt;gpiochip_add: registered GPIOs 96 to 127 on device: imx31-gpio.3&lt;/P&gt;&lt;P&gt;gpiochip_add: registered GPIOs 128 to 159 on device: imx31-gpio.4&lt;/P&gt;&lt;P&gt;gpiochip_add: registered GPIOs 160 to 191 on device: imx31-gpio.5&lt;/P&gt;&lt;P&gt;gpiochip_add: registered GPIOs 192 to 223 on device: imx31-gpio.6&lt;/P&gt;&lt;P&gt;hw-breakpoint: debug architecture 0x4 unsupported.&lt;/P&gt;&lt;P&gt;bio: create slab &amp;lt;bio-0&amp;gt; at 0&lt;/P&gt;&lt;P&gt;SCSI subsystem initialized&lt;/P&gt;&lt;P&gt;Switching to clocksource mxc_timer1&lt;/P&gt;&lt;P&gt;i.MXC CPU frequency driver&lt;/P&gt;&lt;P&gt;msgmni has been set to 1009&lt;/P&gt;&lt;P&gt;Block layer SCSI generic (bsg) driver version 0.4 loaded (major 254)&lt;/P&gt;&lt;P&gt;io scheduler noop registered&lt;/P&gt;&lt;P&gt;io scheduler deadline registered&lt;/P&gt;&lt;P&gt;io scheduler cfq registered (default)&lt;/P&gt;&lt;P&gt;Serial: IMX driver&lt;/P&gt;&lt;P&gt;imx21-uart.0: ttymxc0 at MMIO 0x53fbc000 (irq = 31) is a IMX&lt;/P&gt;&lt;P&gt;console [ttymxc0] enabled&lt;/P&gt;&lt;P&gt;imx21-uart.1: ttymxc1 at MMIO 0x53fc0000 (irq = 32) is a IMX&lt;/P&gt;&lt;P&gt;imx21-uart.3: ttymxc3 at MMIO 0x53ff0000 (irq = 13) is a IMX&lt;/P&gt;&lt;P&gt;imx21-uart.4: ttymxc4 at MMIO 0x63f90000 (irq = 86) is a IMX&lt;/P&gt;&lt;P&gt;loop: module loaded&lt;/P&gt;&lt;P&gt;i2c /dev entries driver&lt;/P&gt;&lt;P&gt;sdhci: Secure Digital Host Controller Interface driver&lt;/P&gt;&lt;P&gt;sdhci: Copyright(c) Pierre Ossman&lt;/P&gt;&lt;P&gt;sdhci-pltfm: SDHCI platform and OF driver helper&lt;/P&gt;&lt;P&gt;mmc0: SDHCI controller on sdhci-esdhc-imx53.0 [sdhci-esdhc-imx53.0] using DMA&lt;/P&gt;&lt;P&gt;VFP support v0.3: implementor 41 architecture 3 part 30 variant c rev 2&lt;/P&gt;&lt;P&gt;Waiting for root device /dev/mmcblk0p1...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;regards&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;Nicolas K&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 25 Sep 2012 14:40:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX53-boot-on-SD-Card/m-p/200140#M10912</guid>
      <dc:creator>nicolask</dc:creator>
      <dc:date>2012-09-25T14:40:47Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX53 boot on SD Card</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX53-boot-on-SD-Card/m-p/200141#M10913</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;some topics to care about:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;* Is your sdcard hardware OK?&lt;/P&gt;&lt;P&gt;* Does sdcard work on u-boot?&lt;/P&gt;&lt;P&gt;* Does your kernel has SDCard enabled?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 25 Sep 2012 19:55:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX53-boot-on-SD-Card/m-p/200141#M10913</guid>
      <dc:creator>daiane_angolini</dc:creator>
      <dc:date>2012-09-25T19:55:34Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX53 boot on SD Card</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX53-boot-on-SD-Card/m-p/200142#M10914</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;the sdcard hardware work fine u-boot is ok (read partition ext2 ok, writing env variables ok on SD Card)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;the kernel had an SD Card enabled.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;After a new verifications and another try, I found the CD signal for the SD Card is not asserted.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank's for your answer,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;regards&lt;/P&gt;&lt;P&gt;Nicolas K&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 26 Sep 2012 05:45:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX53-boot-on-SD-Card/m-p/200142#M10914</guid>
      <dc:creator>nicolask</dc:creator>
      <dc:date>2012-09-26T05:45:58Z</dc:date>
    </item>
  </channel>
</rss>