<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic frame rate issue in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/frame-rate-issue/m-p/702061#M109076</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hai;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;currently i am working under imx6 processor with parallel camera module ,i done the camera interface and live streaming also,but only we got 15 fps as per my requirement i need achive minimum of 30 fps ,so kindly provided any solution to over come this problem and i tried using mxc out but its give QBUF and DQBUF .&lt;/P&gt;&lt;P&gt;i am using YUYV format to capture camera data and i converted to &lt;A href="mailto:RGB@4"&gt;RG&lt;/A&gt;B24 using image converter ic &amp;nbsp;and i directly write into frame buffer fbo&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 13 Sep 2017 04:23:49 GMT</pubDate>
    <dc:creator>muralikrishnant</dc:creator>
    <dc:date>2017-09-13T04:23:49Z</dc:date>
    <item>
      <title>frame rate issue</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/frame-rate-issue/m-p/702061#M109076</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hai;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;currently i am working under imx6 processor with parallel camera module ,i done the camera interface and live streaming also,but only we got 15 fps as per my requirement i need achive minimum of 30 fps ,so kindly provided any solution to over come this problem and i tried using mxc out but its give QBUF and DQBUF .&lt;/P&gt;&lt;P&gt;i am using YUYV format to capture camera data and i converted to &lt;A href="mailto:RGB@4"&gt;RG&lt;/A&gt;B24 using image converter ic &amp;nbsp;and i directly write into frame buffer fbo&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 13 Sep 2017 04:23:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/frame-rate-issue/m-p/702061#M109076</guid>
      <dc:creator>muralikrishnant</dc:creator>
      <dc:date>2017-09-13T04:23:49Z</dc:date>
    </item>
    <item>
      <title>Re: frame rate issue</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/frame-rate-issue/m-p/702062#M109077</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Muralikrishnan&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;performance may be affected by IC conversion times, so to narrow down issue one&lt;/P&gt;&lt;P&gt;can try to remove conversion routines or try with baremetal SDK IPU camera tests&lt;/P&gt;&lt;P&gt;Github SDK&lt;BR /&gt;&lt;A class="jive-link-external-small" href="https://community.nxp.com/external-link.jspa?url=https%3A%2F%2Fgithub.com%2Fbackenklee%2Fswp-report%2Ftree%2Fmaster%2FiMX6_Platform_SDK" rel="nofollow" target="_blank"&gt;https://github.com/backenklee/swp-report/tree/master/iMX6_Platform_SDK&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 14 Sep 2017 02:03:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/frame-rate-issue/m-p/702062#M109077</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2017-09-14T02:03:42Z</dc:date>
    </item>
  </channel>
</rss>