<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックADC input</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/ADC-input/m-p/701450#M108965</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, I'm trying to configure the internal ADC for i.MX6ULL. How I can configure pin by software. I use the command echo 1 &amp;gt; /sys/class/gpio/export for digital I/O. Is there something similar?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 09 Oct 2017 15:29:52 GMT</pubDate>
    <dc:creator>jacopoagostini</dc:creator>
    <dc:date>2017-10-09T15:29:52Z</dc:date>
    <item>
      <title>ADC input</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/ADC-input/m-p/701450#M108965</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, I'm trying to configure the internal ADC for i.MX6ULL. How I can configure pin by software. I use the command echo 1 &amp;gt; /sys/class/gpio/export for digital I/O. Is there something similar?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 09 Oct 2017 15:29:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/ADC-input/m-p/701450#M108965</guid>
      <dc:creator>jacopoagostini</dc:creator>
      <dc:date>2017-10-09T15:29:52Z</dc:date>
    </item>
    <item>
      <title>Re: ADC input</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/ADC-input/m-p/701451#M108966</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Jacopo&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;please look at available options described in sect.53.3.3 Programming Interface&lt;/P&gt;&lt;P&gt;attached Linux Manual. Pins can be configured using dts pinctrl_adc1: adc1grp entry:&lt;/P&gt;&lt;P&gt;&lt;A class="" href="http://git.freescale.com/git/cgit.cgi/imx/linux-imx.git/tree/arch/arm/boot/dts/imx6ull-14x14-ddr3-arm2.dts?h=imx_4.9.11_1.0.0_ga" title="http://git.freescale.com/git/cgit.cgi/imx/linux-imx.git/tree/arch/arm/boot/dts/imx6ull-14x14-ddr3-arm2.dts?h=imx_4.9.11_1.0.0_ga"&gt;http://git.freescale.com/git/cgit.cgi/imx/linux-imx.git/tree/arch/arm/boot/dts/imx6ull-14x14-ddr3-arm2.dts?h=imx_4.9.11_…&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 10 Oct 2017 05:01:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/ADC-input/m-p/701451#M108966</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2017-10-10T05:01:42Z</dc:date>
    </item>
  </channel>
</rss>