<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic qt app too small for screen resolution in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/qt-app-too-small-for-screen-resolution/m-p/701191#M108925</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;hi,&lt;/P&gt;&lt;P&gt;i got matchbox installed and the qt examples. My screen has a resolution of 1280x800, but when i start a qt example app after boot, e.g. qtsmarthome directly from a /home/user/.matchbox/session file, it only displays the qtsmarthome only in 800x480 size ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I changed the width and heigth settings inside &amp;nbsp;qtsmarthome-1.0/qml/smarthome/smarthome.qml &amp;nbsp;file to 1280x800, but nothing changed ? &amp;nbsp;I also changed DISPLAY_WIDTH_PIXELS and DISPLAY_HEIGHT_PIXELS inside /etc/formfactor/machconfig &amp;nbsp;but also nothing changed ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I start the qtsmarthome app with the line:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;/usr/share/qtsmarthome-1.0/smarthome --platform xcb&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The interresting thing is, when i start smarthome from cmdline without the matchbox session file, it starts in big resolution, but not fullscreen , because of the matchbox-panel at the top of the screen.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;How can i setup the correct resolution to start a qt example app right after booting in fullscreen ?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 17 Aug 2017 14:18:27 GMT</pubDate>
    <dc:creator>floriankoenig</dc:creator>
    <dc:date>2017-08-17T14:18:27Z</dc:date>
    <item>
      <title>qt app too small for screen resolution</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/qt-app-too-small-for-screen-resolution/m-p/701191#M108925</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;hi,&lt;/P&gt;&lt;P&gt;i got matchbox installed and the qt examples. My screen has a resolution of 1280x800, but when i start a qt example app after boot, e.g. qtsmarthome directly from a /home/user/.matchbox/session file, it only displays the qtsmarthome only in 800x480 size ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I changed the width and heigth settings inside &amp;nbsp;qtsmarthome-1.0/qml/smarthome/smarthome.qml &amp;nbsp;file to 1280x800, but nothing changed ? &amp;nbsp;I also changed DISPLAY_WIDTH_PIXELS and DISPLAY_HEIGHT_PIXELS inside /etc/formfactor/machconfig &amp;nbsp;but also nothing changed ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I start the qtsmarthome app with the line:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;/usr/share/qtsmarthome-1.0/smarthome --platform xcb&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The interresting thing is, when i start smarthome from cmdline without the matchbox session file, it starts in big resolution, but not fullscreen , because of the matchbox-panel at the top of the screen.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;How can i setup the correct resolution to start a qt example app right after booting in fullscreen ?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 17 Aug 2017 14:18:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/qt-app-too-small-for-screen-resolution/m-p/701191#M108925</guid>
      <dc:creator>floriankoenig</dc:creator>
      <dc:date>2017-08-17T14:18:27Z</dc:date>
    </item>
  </channel>
</rss>