<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 video clock timings during kernel logo</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/video-clock-timings-during-kernel-logo/m-p/700834#M108857</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I use an LCD with a pixel clock of 33MHz.&amp;nbsp; I set my source to pll5 in clk-imx6q.c to allow a clock lower than 38MHz.&lt;/P&gt;&lt;P&gt;I also display a logo from the kernel.&lt;/P&gt;&lt;P&gt;However, during the logo display, the pixel clock measure approx. 8MHz.&lt;/P&gt;&lt;P&gt;After the kernel boots, the pixel clock is 33MHz as desired.&lt;/P&gt;&lt;P&gt;How can I correct the initial pixel clock?&lt;/P&gt;&lt;P&gt;I am using an iMX6q, Linux 3.10.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 12 Sep 2017 16:07:48 GMT</pubDate>
    <dc:creator>bblock72</dc:creator>
    <dc:date>2017-09-12T16:07:48Z</dc:date>
    <item>
      <title>video clock timings during kernel logo</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/video-clock-timings-during-kernel-logo/m-p/700834#M108857</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I use an LCD with a pixel clock of 33MHz.&amp;nbsp; I set my source to pll5 in clk-imx6q.c to allow a clock lower than 38MHz.&lt;/P&gt;&lt;P&gt;I also display a logo from the kernel.&lt;/P&gt;&lt;P&gt;However, during the logo display, the pixel clock measure approx. 8MHz.&lt;/P&gt;&lt;P&gt;After the kernel boots, the pixel clock is 33MHz as desired.&lt;/P&gt;&lt;P&gt;How can I correct the initial pixel clock?&lt;/P&gt;&lt;P&gt;I am using an iMX6q, Linux 3.10.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 12 Sep 2017 16:07:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/video-clock-timings-during-kernel-logo/m-p/700834#M108857</guid>
      <dc:creator>bblock72</dc:creator>
      <dc:date>2017-09-12T16:07:48Z</dc:date>
    </item>
    <item>
      <title>Re: video clock timings during kernel logo</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/video-clock-timings-during-kernel-logo/m-p/700835#M108858</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Dave&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;please look at patches provided on&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-98109"&gt;Patch to support uboot logo keep from uboot to kernel for NXP Linux and Android BSP (HDMI, LCD and LVDS)&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 12 Sep 2017 23:04:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/video-clock-timings-during-kernel-logo/m-p/700835#M108858</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2017-09-12T23:04:49Z</dc:date>
    </item>
  </channel>
</rss>